I am encountering an issue while trying to configure the mainsecondary I2C interface (MP24/SCL, MP25/SDA) on my ADAU1467 to read from an external I2C device.
In my SigmaStudio project, I have an "I2C Continuous Read" block connected to a "DSP Readback" block. My goal is to continuously read data from a specific register on the external device.

The external I2C device has a 7-bit address of 0x40 (hexadecimal). According to the I2C protocol, for a read operation, the 8th bit of the address should be '1'. I need to read data from register 0x01 (hexadecimal) of this device.

However, when I monitor the I2C bus, I observe that the ADAU1467 is sending the device address 0x80 (hexadecimal). This corresponds to the 7-bit address 0x40 with the 8th bit as '0', indicating a write operation. Consequently, my external device is not responding as expected to a read request.

Could you please advise on why the ADAU1463 is sending a write address (0x80) when the "I2C Continuous Read" block is configured for reading from the device at address 0x40? Is there a specific setting or consideration within SigmaStudio or the ADAU1467's I2C configuration that I might be overlooking to ensure the correct read address (0x81) is transmitted?
Any insights or suggestions on how to resolve this issue would be greatly appreciated. Thank you for your time and assistance.