Post Go back to editing

SigmaStudio+ Master control block doesn't work (same xml as SigmaStudio 4.7?)

Category: Software
Product Number: ADAU1466
Software Version: 2.3

Hello,

I moved my project from SS 4.7 to SS+ 2.3 because checksum errors, and now I'm dealing with several problems. My actual is the Master Control Port Block

I made a test project with just this:

 

A configuration for the PCA9536 and a Control Port with external trigger, but is not working.

I confirm that is working because the same XML, same block work with the SS 4.7.

The XML config code:

The XML test code, to turn on all outputs:

Someone can confirm the XML is the same as used in the SS 4.7?


Thanks!

Edit Notes

Just the end
[edited by: IcaroViana2 at 8:34 PM (GMT -4) on 19 Mar 2025]
Parents
  • Hello ,

    We will check this and get back to you, thanks.

    Regards 

    Harish 

  • Any news, Harish? I tried many things too, but none of them worked… maybe a software problem, xml incompatibility, don’t know 

  • Hello,

    Sorry for the trouble caused, it does seem like a bug, but I have to double check it before commenting further. I have tried it too and encountered some strange behaviors.

    The self-boot function and other read and write with the EEPROM works fine, the EEPROM is connected with MP0. I wrote a program to the EEPROM and self-booted it, and I can use the SPI read block from master control port to read first four bytes of the EEPROM successfully.

    However, If I use other slave selects (MP pins) for writing to external chips like codec etc., then it doesn't work. I can see commands going out, but it doesn't program the external chip.

    I have also tried to program the codec on the ADAU1467Z board with an XML file by I2C, it didn't work too. (Here I can't see any commands going out). whereas the same XML file and setup worked fine with SS. 

    So, I don't think it's your problem, I guess the issue exists with SS+. I will have to investigate this further.

    UPDATE: I have been experimenting with the master control port blocks, so I will update it soon after some necessary testing is done. 

    Regards,

    Harish

  • Ty!

    i’ll wait a fix, maybe a new version of the SS+, don’t know. If there is any news, tell me.

    For while, I’ll go back to SS (that I have another several problems, but works when it wants)

Reply Children
No Data