Post Go back to editing

Regarding the behavior of the adau1772 evaluation board

Category: Hardware
Product Number: ADAU1772

Hello. I recently purchased and am using the adau1772 evaluation board.

The power to the eval board is powered by USB.
For the input signal, I input a signal with OFFSET=0V, AMPLITUDE=500mV to AIN0 of J11 through a function generator. Also, to see the output, I am using it by connecting CLASS AB audio amp -> speaker to J23 in that order.
(Overall structure: function generator -> adau eval board -> audio amp -> speaker)
(The positions of each jumper are the settings that were delivered when it was first installed.)

When I first operated it as above, the sound was output well and various functions (inverting, PGA, etc.) on Sigma Studio worked well.

But suddenly, the appropriate address for operation is not entered in the register, and even if the appropriate address is entered, the sound is not output.

It may seem like a silly question, but I have no idea why it doesn't work.

I'm attaching the SigmaStudio file I used and a picture of the board.

Thank you.design1.dspproj

Parents
  • +++

    When measuring AIN0 of adau1772 chip with OSC, I confirmed that the signal input to the function generator was input. However, when measuring RP/LOUTRP, which is thought to be the output pin of adau1772 chip with OSC, no signal was measured.

    DVDD measured 1.26V.
    CM measured 1.65V.

  • Hello YEONGJI,

    you somehow turned on the Selfboot function which will cause problems if it is not programmed. 

    On this part it will also lock up the USBi if you try to program it so if you get the "compiled Comms Failed" message on the bottom right of the screen. Then unplug the USBi from the USB port and reinsert it, then try to program the part after you turn off the selfboot switch.

    I verified this on my board using your program. 

    Dave T

  • Hello. Thank you for your answer.

    However, I still have a problem with the operation.

    I turned off selfboot and tried to operate the board yesterday. However, when I upload (F7), the sound for the input signal is output for about 1-2 seconds and the board turns off immediately.

    Q1) When the sound is output for 1-2 seconds, the numbers from the first to the 10th byte are different from when it doesn't work. Is this normal?

    Q2) When I first bought the board, I confirmed that it worked well, but now it doesn't work well even with the same settings as before. Could it be a board failure? I don't know what else to try.

Reply
  • Hello. Thank you for your answer.

    However, I still have a problem with the operation.

    I turned off selfboot and tried to operate the board yesterday. However, when I upload (F7), the sound for the input signal is output for about 1-2 seconds and the board turns off immediately.

    Q1) When the sound is output for 1-2 seconds, the numbers from the first to the 10th byte are different from when it doesn't work. Is this normal?

    Q2) When I first bought the board, I confirmed that it worked well, but now it doesn't work well even with the same settings as before. Could it be a board failure? I don't know what else to try.

Children