Post Go back to editing

Instructions (Cycles) close to 100% sometimes does not pass audio

Category: Hardware
Product Number: ADAU1452

I am running the ADAU1452 with a program that has worked in the past. The compiler was at 98% of Inst cycles, I added a few more EQ blocks, and the % is at 99%. I have had a few cases where the audio is not passing through the system when it was OK at first boot, and I am trying to track down the problem. Is it possible that the program, when executed is actually over 100% and the program cannot properly run?