I'm using a ADAU1701 to do some analysis on the frequency content of the ADC input then pull those readings into my MCU. I've had no problem performing a readback of a single level detector value, as the value register is apparent. I've now built a multiple band pass-through level detector to in hope to readback the values at each band but it's not so clear what register I should be reading to pull back a value. Let me know if this approach makes sense and if there is a way to determine what register I should be reading from.