I really need help on this or my boombox project is dead in the water!
Here is a link to the 2-way project file I downloaded from HiFiBerry: https://www.hifiberry.com/wp-content/uploads/2017/10/2-way-eq.dspproj.zip . However, the only difference between the screenshot below and the project file I originally downloaded and modified is the 2way crossovers I added just before the outputs (and they work as intended).
But there is know SPIDF output in the sample project file I started with and modified, so adding the SPIDF output it is what I need help with. I already bought a DAC with optical/SPIDF input and two (left & right) RCA outputs to power a separate subwoofer amplifier I also purchased.
Preferably, I need a two channel SPIDF output added (or at least screenshots on how to add it myself).