Post Go back to editing

How do I modify this 2way project file to get the SPIDF output working on my HiFiBerry Beocreate 4ch amplifier?

Category: Hardware
Product Number: ADAU1451

I really need help on this or my boombox project is dead in the water! 

Here is a link to the 2-way project file I downloaded from HiFiBerry: https://www.hifiberry.com/wp-content/uploads/2017/10/2-way-eq.dspproj.zip . However, the only difference between the screenshot below and the project file I originally downloaded and modified is the 2way crossovers I added just before the outputs (and they work as intended).

But there is know SPIDF output in the sample project file I started with and modified, so adding the SPIDF output it is what I need help with. I already bought a DAC with optical/SPIDF input and two (left & right) RCA outputs to power a separate subwoofer amplifier I also purchased. 

Preferably, I need a two channel SPIDF output added (or at least screenshots on how to add it myself).









Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.