Post Go back to editing

Analog ports not <orking anymore

Category: Hardware
Product Number: ADAU1467

Hello,

I am using the ADAU1467 eval board to test the audio signals on a Bluetooth module. The setup is simple as shown in the following picture :

I input the audio directly through the IN0 serial port pins. The output is set to the analog output 1. Until now, everything worked correctly. However, at some point, I changed one parameter that I had changed multiple times before (the input/output I2S clocks) in the serial port registers, and when I compiled, I couldn't hear any audio anymore. I have tried reverting to prior changes but the issue is still there. To make sure that I didn't mess with any registers, I started a blank project with the same configuration. The only parameters I changed are the MCLK frequency that I set to 128*Fs to have the same frequency as my Bluetooth module, as well as the input0 clocks that I set to slaves from domain0 for either BCLK and LRCLK. Unfortunately, the analog ports don't seem to work anymore (wether it's for input or output). I can confirm that the serial input pins function correctly based on the levels I used in my config.

I have noticed that one detail on the USBi card that I use to program the ADAU. Upon connecting it to my computer, the I2C LED turns on as usual, but after a few seconds, the SPI LED starts blinking as if it weren't powered properly. I don't know if the issue originates from the USBi card.

Would anyone know where the issue could come from (hoping that the ADAU board isn't dead).

ThibDouil

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.