AD1939
Production
The AD1939 is a high performance, single-chip codec that provides four analog-to-digital converters (ADCs) with differential input, and eight digital-to...
Datasheet
AD1939 on Analog.com
AD1938
Production
The AD1938 is a high performance, single-chip codec that provides four analog-to-digital converters (ADCs) with input and eight digital-to-analog converters...
Datasheet
AD1938 on Analog.com
I've just built my first circuit/PCB with an AD1939 codec. Powered up and have checked for shorts in the circuit etc... Connected my USBi device (from an eval' board) and setup a quick SigmaStudio program with the AD193x device. Whenever I try to write to device or read the settings from the chip I get "Compiled, Comms Failed". Where should I start fault finding this so I can configure my AD1939? Any ideas greatly received!
Kind regards,
Mark
Image of my board (excuse the over bright LED's... whoops!):