- Hi. I'm using an ADAU1701 with I2S input and DAC output as an active crossover. It takes I2S from a Bluetooth module with 6.122MHz BCLK and 96kHz LRCLK. It also has a 12.288MHz oscillator as master clock. In Sigma Studio, I've set the PLL to 256 and core rate to 2x256. What's happening is that the signal appears on the VOUT with a sort of LPF response at 12dB/decade starting from a very low frequency, about 100Hz. It was measured directly on the VOUT pins. Just for testing purposes, in Sigma Studio I have made a direct connection from the I2S input to VOUT, but I still get this "phantom" LPF response. Am I doing something wrong? I forgot to say that the I2S is reclocked using a 74HC574 before going to the ADAU1701. Thanks.