Post Go back to editing

Modifying saved config in an existing system

Category: Hardware
Product Number: ADAU1701

Hi,

I'm looking at putting some active power amp modules into some of my passive loudspeaker systems.

I've been able to track down some suitable "complete build" modules that should simply drop in to the cabinets. However, the pre-programmed EQ and crossover curves are unsuitable for my speakers/cabinets and I wish to change them.

The manufacturer of the modules has not been helpful so I thought that since the processor is made by AD, I might be able to change things myself.

Since the ADAU1701 processor is already on the main circuit board, is there a way to make a small modification that will allow me communication access so that I can change these parameters? I've been looking through the SigmaStudio software but at first glance there does not seem to be a way to dump the config out so that I can make a change and put it back.

Has anyone done this? If so, how did you configure an interface to communicate with the device and is is possible to get the config out to change it since the device is soldered to the existing board?

This seems like something that would be possible to achieve but I don't really know where to start. Can anyone point me in the right direction? Thanks.