HI ADI's
One of my customers wants to implement the following functionality.
1. Digital audio input must be capable of buffering for up to 8 seconds.
Since all audio inputs are 4ch (16bit & 48kHz), the total time required for buffering is 32 seconds. (Use of external RAM is also being considered)
*1ch is mono.
2. The Time Stretching function is required to speed up the playback speed of the buffered audio signal to 1.0~3.0 times.
Does SigmaDSP have a solution that can implement the above function?
Thank you