ADAU1466
Production
The ADAU1462/ADAU1466 are automotive qualified audio processors that far exceed the digital signal processing capabilities of earlier SigmaDSP® devices...
Datasheet
ADAU1466 on Analog.com
If you need to use the audio source i2s input port0, i2s output port1
How to set up in SIGMA STUDIO GUI?
Hello,
Please find the attached pass thru program. Since you didn't mention what sample rate you are using, I just set it up for the default rate which is 48kHz. PLL settings are also set as default which is for 12.288MHz MCLK_IN.
Kindly do reply, if you have any questions.
Regards,
Harish
Hello,
Please find the attached pass thru program. Since you didn't mention what sample rate you are using, I just set it up for the default rate which is 48kHz. PLL settings are also set as default which is for 12.288MHz MCLK_IN.
Kindly do reply, if you have any questions.
Regards,
Harish