Post Go back to editing

EVAL-ADAU1787Z USB Communication Failure Error

Category: Software
Product Number: EVAL-ADAU1787, ADAU1787, ADAU1787
Software Version: SigmaStudio 4.7

Dear ADI team,

I encountered the same problem as below link,

 EVAL-ADAU1787Z USB Communication Failure Error 

How can I do now?



Added pictures
[edited by: ElvisJ at 3:11 AM (GMT -4) on 8 May 2024]
Parents
  • Hello ElvisJ,

    Thanks for the pictures and screenshots. From what I can see nothing is standing out to me as the problem. The first thing I would like for you to test is if the USBi is set to 1.8V verses 3.3V? It is a small slide switch on the bottom of the board. This will cause this issue. 

    Then if you can take some more picture from slightly different angles and closer up of the eval board so we can see all the jumper positions? I can see some of them but not certain about a few where it is difficult to see. 

    It looks like you have the correct address settings...

    Dave T

Reply
  • Hello ElvisJ,

    Thanks for the pictures and screenshots. From what I can see nothing is standing out to me as the problem. The first thing I would like for you to test is if the USBi is set to 1.8V verses 3.3V? It is a small slide switch on the bottom of the board. This will cause this issue. 

    Then if you can take some more picture from slightly different angles and closer up of the eval board so we can see all the jumper positions? I can see some of them but not certain about a few where it is difficult to see. 

    It looks like you have the correct address settings...

    Dave T

Children