ADAU1761
Production
The ADAU1761 is a low power, stereo audio codec with integrated digital audio processing that supports stereo 48 kHz record and playback at 14 mW from...
Datasheet
ADAU1761 on Analog.com
ADAU1961
Production
The ADAU1961 is a low power, stereo audio codec that supports stereo 48 kHz record and playback at 35 mW from a 3.3 V analog supply. The stereo audio ADCs...
Datasheet
ADAU1961 on Analog.com
Hi,
We use the ADAU1961WBCPZ
In the Jtag station we check the digital signal of our system.
The Codec ADAU1961WBCPZ does not have Jtag lines. However we use to toggle the lines in Boundary scan and thus test the devices that do not have Jtag.
For the ADAU1961WBCPZ we tests the I2C lines by reading and writing to register thus verifying the i2C bus integrity.
I want to add additional test that check the I2S ADCsdata and the clocks.
See in red the idea :
Thanks,
Freddy for Avner
Hello Freddy,
No, there is no way to do this on this part. If you were using the ADAU1761 which has the DSP core then you can create a program that loops the serial input over directly to the serial output but with the codec only part there is no loopback function.
The only way to do something kind of like this is to setup a jumper external to the part to take the DAC output and feed it back to the ADC inputs. Then send data to the DACs and see what the serial data output of the ADC looks like.
You could have this done as a manual test by having an operator connect an external jumper to loop the audio back in. We have done that to test eval boards at the factory. You just have to make sure there is no feedback path to cause an infinite loop.
Dave T
Hello Freddy,
No, there is no way to do this on this part. If you were using the ADAU1761 which has the DSP core then you can create a program that loops the serial input over directly to the serial output but with the codec only part there is no loopback function.
The only way to do something kind of like this is to setup a jumper external to the part to take the DAC output and feed it back to the ADC inputs. Then send data to the DACs and see what the serial data output of the ADC looks like.
You could have this done as a manual test by having an operator connect an external jumper to loop the audio back in. We have done that to test eval boards at the factory. You just have to make sure there is no feedback path to cause an infinite loop.
Dave T