Post Go back to editing

Equivalent t connector in sigma studio+

Category: Software
Product Number: ADAU1452
Software Version: Sigma Studio+ 2.0

I am upgrading a schematic drawing for a ADAU1452 from Sigma Studio 4.7 to Sigma Studio+ 2.0. The import feature did not work, trying to open the schematic would lock up Sigma Studio+, so I am redrawing the design. What is the equivalent t connection for sigma studio+? I found the simple router and block splitter, but I am not sure if one or both behaves like the t connection that does not use DSP resources and is established at compile/link time.

Parents
  • Hello kernel757,

    I think you are asking about the T-connection" that sigmaStudio uses to "Y" a connection to several places? For SS+ it is sort of designed in. In the old SigmaStudio you could only connect one wire to a pin, in SS+ you can connect multiple wire to the same output creating the same thing you would use the "T" for. 

    That is what I did here:

    Two wires are connected to the same pin. You can only do this with an output pin of course. You cannot "mix two signals onto one pin unless you use a summing block. 

    Dave T

Reply
  • Hello kernel757,

    I think you are asking about the T-connection" that sigmaStudio uses to "Y" a connection to several places? For SS+ it is sort of designed in. In the old SigmaStudio you could only connect one wire to a pin, in SS+ you can connect multiple wire to the same output creating the same thing you would use the "T" for. 

    That is what I did here:

    Two wires are connected to the same pin. You can only do this with an output pin of course. You cannot "mix two signals onto one pin unless you use a summing block. 

    Dave T

Children
No Data