Post Go back to editing

Dayton audio KABD-430 configuration

Category: Software

Is it possible to use all 4 DAC and the 2 DIG outputs at the same time on a KABD-430?  I want to use a 3 way crossover where the output for the Hi go to DAC0 and DAC1. Outputs for the Lo go to DAC2 and DAC3. Outputs for the Mid go to DIG0 and DIG1.

Parents
  • Hello Vimocam,

    I do not have one of these boards and I just looked for the schematic. If you can find a schematic then look to see two things:

    1) Are they using the needed MP pins for other uses?

    2) Did they bring out the MP pins to somewhere such that you can solder to them to make the connections? 

    Here is the register settings for a project that is is using both the digital input and output. 

    For only digital output you will need to use MP6, MP10, MP11

    Dave T

Reply
  • Hello Vimocam,

    I do not have one of these boards and I just looked for the schematic. If you can find a schematic then look to see two things:

    1) Are they using the needed MP pins for other uses?

    2) Did they bring out the MP pins to somewhere such that you can solder to them to make the connections? 

    Here is the register settings for a project that is is using both the digital input and output. 

    For only digital output you will need to use MP6, MP10, MP11

    Dave T

Children
No Data