Post Go back to editing

Compressor input level appears to be displayed/calculated incorrectly

Thread Summary

The user encountered inconsistent input level readings on the compressor block (Dynamic Processors/Peak/Standard/Full Range/Standard Peak) in SigmaStudio, affecting compression calculations. The support engineer explained that the compressor's level meter is not an absolute reference and is influenced by the absolute value of the audio and time constants. A workaround involves using external meters for more accurate level monitoring. The issue is also related to the compressor's gain factor calculation, which can be adjusted using a sidechain input with a volume control for threshold changes.
AI Generated Content
Category: Software
Product Number: ADAU1452
Software Version: SS 4.6, 4.7

During some recent work, I have been using one of the compressor blocks (Dynamic Processors/Peak/Standard/Full Range/Standard Peak). I noticed the "IN" Level displayed on the level indicators appears to be inconsistent with the level detector block (Level Detectors/Level Detectors/Single Band/Single Level Detector w Numerical Display). I am worried that this means that the amount of compression is being incorrectly calculated.

To isolate the problem, I have created a minimum working example, which is both attached and screenshotted below.

The input that the compressor displays appears to be negative half the absolute value (in dB) of the louder of the two inputs. (Sorry, that's a poor explanation)

e.g. Input 1 is -63dB, Input 2 is -56dB, compressor displays -28dB. This is because  -28 = - abs(-56)/2.

I don't know if this is exactly what is happening within the compressor, but I do know that the compressor is the issue, as increasing the linear gain value to 2 in the external gain block, which should lead to a 6dB increase, increases the compressor input level by 3dB.

For reference the ADAU1452 is on the Analog Devices EVAL-ADAU1452 REV BZ board. I have used the analog inputs to the board to test this, but the problem also appears with the noise floor of the ADCs, so no audio is needed. The included image was taken with only the noise of the ADC passing through the DSP. I have tried the same project on the two latest version of SigmaStudio (4.6, 4.7), with the same results in both cases.

Have I made a mistake in my setup, or is this a problem with the compressor?

Thanks,

Alex  

Edit Notes

Edit: The image and file that I attached appear to have been removed, and I cannot seem to add them back.
[edited by: AlexHolt at 12:14 PM (GMT -4) on 20 Oct 2022]
Parents
  • Hello Alex,

    For the picture issue, you might want to try to either copy and paste the picture file or drag and drop it into the window. 

    The compressor meter is certainly not perfect and is there to give you an idea of what is going on and not be an absolute reference level. 

    The compressor code will take the audio and it takes the absolute value of the audio and then it uses time constants to allow the level to build slowly and release slowly to get the attack and release times. So the result is a level that is used to lookup the gain factor to apply to the audio. So any non-symmetrical signals will get properly measured.

    As far as the level meters in the compressor. A couple of years ago I did look into the code that drives the meters and there are some issues with how it is displayed. It is not the actual audio output. Again, these meters are just to give you an idea of what the levels are. 

    Try to put a meter on the input and one on the output of the compressor. This should give you a better idea of the level in and out. 

    I had put together this document a few years back. It does not exactly explain what you are asking about but it does show how the parameters all work.

    Can you put together a small project that shows the issue you are seeing? 

    Dave T

    PDF 

     

  • Hi Dave,

    Thanks for the reply.

    I think that about answers my question.

    I encountered this in a larger project, and the image that I posted on 21st October shows my minimum working example project in its entirety.

    Best,

    Alex

Reply Children
No Data