Post Go back to editing

ADAU1467 - Suppression of Mechanical Noise and use of two microphones

Hi all,

I want to achieve the effect of active noise cancellation (ANC) for the recognition of the human voice with mechanical noise from machine tools and engines (according to the design of the post attached at the bottom). I use two microphones for the device where the 1st mic is dynamic (main microphone) and the 2nd mic is electret with preamplifier (reference microphone).
Application:
- voice transmission;
- suppression of noise received by the main microphone.

I conducted an experiment on EVAL-ADAU1467Z with the provided project and achieved probably some minimal result. Some effect was present but the noise in the vocal range was not suppressed, so the person's voice could not be heard clearly. What can you recommend to solve this situation?

The reference microphone is placed at a distance of 50 cm from the main microphone. Type of noise - mechanical (machine tools, engines, etc.).

Figure1 - Block diagram

Figure 2 - Approximate representation of the complete structure

Figure 3 - Photo (complete design unfortunately does not fit in the photo)

NLMS filter-DT-Edits.dspproj

Regards,

Artem (Fox108).

Parents
  • Hello,

    I looked at your project, you are using an adaptive line enhancer (ALE) method, which works well for suppressing stationary narrowband interference (i.e. tones) from a broadband signal (i.e. speech). If the interference has a broadband component in the same range as the speech it will not be suppressed. You can observe this in the attached modified project, unwanted tones are suppressed but noise is not suppressed.

    NLMS filter-DT-Edits_modified.dspproj

  • I think a possible solution is shown in the attached figure. The noise is present at both the ref mic and main mic and will be removed from the main mic by the NLMS. Note when speech is present you need a voice activity detector (VAD) to freeze the NLMS. VAD can be very tricky, but in this case perhaps when energy level at main mic is above a threshold assume speech is present and freeze the NLMS. Also, this assumes the ref mic does not pick up the speech.

Reply
  • I think a possible solution is shown in the attached figure. The noise is present at both the ref mic and main mic and will be removed from the main mic by the NLMS. Note when speech is present you need a voice activity detector (VAD) to freeze the NLMS. VAD can be very tricky, but in this case perhaps when energy level at main mic is above a threshold assume speech is present and freeze the NLMS. Also, this assumes the ref mic does not pick up the speech.

Children