Hello, there. The card I designed includes 2 ADAU1701, 3 tanae EEPROM and 1 processor. They are on the only I2C line to communicate with each other. I've made and run software for 1 Adau in the Sigma studio app. But 2. Adauya code is not going. The device is not connected error. How do I solve this? Do I have to do the software for two candidates in one project when I create the project? If you have a source document on this issue, can you pass it on? What should I do?
1.ADAU1701 Address 0x68
2.ADAU1701 Address 0x6A
1.EEPROM address 0xA6
2.eeprom address 0xA0
3.EEPROM 0xA8