Post Go back to editing

ADAU1467 EVAL BOARD I2C CONNECTION

I got EVAL-ADAU1467Z REV B board recently. I have couple of problems:

1- I need circuit schematics of this board.

2- I 'm able to load and run ADAU1467 by MCU via SPI connection. it seems analog outputs of AD1937 is fine with sampling rate 48Khz. I need to increase sampling rate 192KHz. To get correct signal at CODEC outputs I need to change register settings of AD1937 as well. I made connection J6/1(SCL) and J6/3(SDA) to MCU. S2 switch is CODEC BOOT MODE. Unfortunately I Have not able to read register contents of AD1937 nor abble to write AD1937 registers. I realy dont understand what 's missing. 

3- Do I have to set some registers on ADAU1467 to communicate between MCU and AD1937 ,it helps if there's sample code for AD1937 I2C communication

Kind Regards,

Parents
  • Hello Husnu,

    We have a more complete answer for you with examples soon. But let me jump in here to answer some things.

    Here is the schematics:

    PDF

    Question 2: 

    The AD1937 is tied to MP24 and MP25 of the DSP. These pins can be set to be the master I2C port. This is to allow the DSP to control and boot up other parts. This is a different I2C port from the slave port. So your MCU is probably connected to the slave port so as to communicate with the DSP. So you will not be able to communicate with the codec that is on another I2C port. So I think that may be the issue here. 

    You can jumper over the I2C lines to the slave port but then you have to change the slave port over to I2C and that is not easy. So the best route is to actually use the DSP to boot up the codec. We will have details on doing that soon. 

    Dave T

  • Hi David,

    I 'm able write and read codec on my eval board by I2C and able to generate signal with 192KHz sampling rate. I have a problem circuit schematics and codec input and output channels:

    1-) I have EVAL-ADAU1467Z 08-0485 Rev.B board. I have required circuit schematics of this board, you probably send me the wrong one because channels’ labels are different:

     

    On My Eval Board

    On Your Schematics

    OUT1

    CH0-CH1

    CH40-CH41

    OUT2

    CH4-CH5

    CH42-CH43

    OUT3

    CH8-CH9

    CH44-CH45

    OUT4

    CH12-CH13

    CH46-CH47

    IN1

    CH32-CH33

    CH40-CH41

    IN2

    CH36-CH37

    CH42-43

     

     

     

     

     

     

     

    Could you please double check which one is correct!

    2-) I’m using eval board with default configuration and SigmaStudio Version 4.6 , and I don’t have any output signal on output channels except CH0-CH1. Do you have any comment !

  • Hello Husnu,

    Sorry for the confusion. I just looked closer at your picture of the PCB and looked through my records and I do not see one that is the same. So I am going to ask Ken for help in this since he is the person who designed these boards. 

    Regarding output on the other jacks. 

    You have to setup the SDATAIO pins that are assignable to output the channels. Channels 4&5, 8&9, and 12&13 are all on serial port 0 and the SDATAIO pins allow access to these upper channels but the serial port has to be setup properly. This information is in the datasheet but I will see if Ken might have an example project.

    Dave T   

Reply
  • Hello Husnu,

    Sorry for the confusion. I just looked closer at your picture of the PCB and looked through my records and I do not see one that is the same. So I am going to ask Ken for help in this since he is the person who designed these boards. 

    Regarding output on the other jacks. 

    You have to setup the SDATAIO pins that are assignable to output the channels. Channels 4&5, 8&9, and 12&13 are all on serial port 0 and the SDATAIO pins allow access to these upper channels but the serial port has to be setup properly. This information is in the datasheet but I will see if Ken might have an example project.

    Dave T   

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.