Post Go back to editing

ADAU1467 EVAL BOARD I2C CONNECTION

I got EVAL-ADAU1467Z REV B board recently. I have couple of problems:

1- I need circuit schematics of this board.

2- I 'm able to load and run ADAU1467 by MCU via SPI connection. it seems analog outputs of AD1937 is fine with sampling rate 48Khz. I need to increase sampling rate 192KHz. To get correct signal at CODEC outputs I need to change register settings of AD1937 as well. I made connection J6/1(SCL) and J6/3(SDA) to MCU. S2 switch is CODEC BOOT MODE. Unfortunately I Have not able to read register contents of AD1937 nor abble to write AD1937 registers. I realy dont understand what 's missing. 

3- Do I have to set some registers on ADAU1467 to communicate between MCU and AD1937 ,it helps if there's sample code for AD1937 I2C communication

Kind Regards,

Parents
  • Hello Husnu,

    We have a more complete answer for you with examples soon. But let me jump in here to answer some things.

    Here is the schematics:

    PDF

    Question 2: 

    The AD1937 is tied to MP24 and MP25 of the DSP. These pins can be set to be the master I2C port. This is to allow the DSP to control and boot up other parts. This is a different I2C port from the slave port. So your MCU is probably connected to the slave port so as to communicate with the DSP. So you will not be able to communicate with the codec that is on another I2C port. So I think that may be the issue here. 

    You can jumper over the I2C lines to the slave port but then you have to change the slave port over to I2C and that is not easy. So the best route is to actually use the DSP to boot up the codec. We will have details on doing that soon. 

    Dave T

Reply
  • Hello Husnu,

    We have a more complete answer for you with examples soon. But let me jump in here to answer some things.

    Here is the schematics:

    PDF

    Question 2: 

    The AD1937 is tied to MP24 and MP25 of the DSP. These pins can be set to be the master I2C port. This is to allow the DSP to control and boot up other parts. This is a different I2C port from the slave port. So your MCU is probably connected to the slave port so as to communicate with the DSP. So you will not be able to communicate with the codec that is on another I2C port. So I think that may be the issue here. 

    You can jumper over the I2C lines to the slave port but then you have to change the slave port over to I2C and that is not easy. So the best route is to actually use the DSP to boot up the codec. We will have details on doing that soon. 

    Dave T

Children
  • Thanks David

    My MCU is connected to J6 port on EVAL board. When I set S2 switch to I2C position I'm able read and write codec. But superior solution will be your advice which DSP will read and write codec. I'll look for examples you will provide soon. Thanks ya lot.

  • Hi David,

    I 'm able write and read codec on my eval board by I2C and able to generate signal with 192KHz sampling rate. I have a problem circuit schematics and codec input and output channels:

    1-) I have EVAL-ADAU1467Z 08-0485 Rev.B board. I have required circuit schematics of this board, you probably send me the wrong one because channels’ labels are different:

     

    On My Eval Board

    On Your Schematics

    OUT1

    CH0-CH1

    CH40-CH41

    OUT2

    CH4-CH5

    CH42-CH43

    OUT3

    CH8-CH9

    CH44-CH45

    OUT4

    CH12-CH13

    CH46-CH47

    IN1

    CH32-CH33

    CH40-CH41

    IN2

    CH36-CH37

    CH42-43

     

     

     

     

     

     

     

    Could you please double check which one is correct!

    2-) I’m using eval board with default configuration and SigmaStudio Version 4.6 , and I don’t have any output signal on output channels except CH0-CH1. Do you have any comment !

  • within https://www.analog.com/media/en/technical-documentation/user-guides/EVAL-ADAU1467Z-UG-1134.pdf on page 38:

    There are two DACR1N/L , one of them is feeding OUTPUT1  and other(probably wrong) is feeding OUTPUT4. Somebody has to check documents before release..

  • Hello Husnu,

    Sorry for the confusion. I just looked closer at your picture of the PCB and looked through my records and I do not see one that is the same. So I am going to ask Ken for help in this since he is the person who designed these boards. 

    Regarding output on the other jacks. 

    You have to setup the SDATAIO pins that are assignable to output the channels. Channels 4&5, 8&9, and 12&13 are all on serial port 0 and the SDATAIO pins allow access to these upper channels but the serial port has to be setup properly. This information is in the datasheet but I will see if Ken might have an example project.

    Dave T   

  • Here is the correct schematic for the Rev B board. Your channel designation (the ones on the silkscreen) are correct:

    PDF

    Here is a project demonstrating how to set the AD1937 CODEC on that board to 192 kHz.

    2642.SigmaDSP Programming CODEC via I2C to 192 kHz.zip

    Lastly, here is a demo project that shows how to configure all of the serial connections for the CODEC. It includes the GPIO and connections necessary for the optional Mic Canvas daughtercard, too, but you can ignore those inputs and configuration of MP24/MP25.

    Preconfigured_project_EVAL-ADAU1467Z_EVAL-MICCANVASZ.zip

    Ken

  • Hello Husnu,

    Regarding the serial port configuration of ADAU1467 Eval board : Like Dave said you can use output channels 4&5,8&9,12&13 and input channels 36&37 with proper serial port setup.Here I have included a project with all set serial ports (input and output channels) of ADAU1467.Hope it will be useful for you.

    Thanks David for your support.ADAU1467 s.port example for eval board 08-048585.dspproj

    Thanks & Regards,

    Harish

  • Hi Ken,

    Thanks your support,

    1-)Circuit Schematic you provided has still wrong labels such as Channelles 40-41 etc.

    2-) I have configured CODEC at 192KHz through I2C and all outputs are working well. When I loop back OUT2 to IN2 I have strange waveform. But When I loop back OUT2 to IN1 output is fine. I have included DSP Project, ADAU1937 Register settings, Block Diagram of my setup and Wafeform at Oscilloscope. Could you have any suggestion Why I'm having strange waveform at OUT3 ?

    King Regards,

    MCU_DSP.rar

  • Hello Dave,

    I had a couple of questions to Ken and not had response yet. it's important to give decision to use ADAu1466 or ADAU1467 in our system. 

    Is there any library for trigonometric functions in Sigma Studio for ADAU1466 or ADAU1467 ?

    Regards,

    Husnu.

  • Sorry for the delay. We had a long holiday weekend here.

    I am a little confused by your question. At first, you say that the problem is OUT2 to IN2, but you later say the strange waveform is on OUT3. You also have a question mark by OUT3 in your diagram. Are you having problems when you connect OUT3 to IN2? In the project, you are connecting IN2 to OUT3 internally, so you will have a feedback loop if you connect OUT3 to IN2 externally. That will, obviously, cause problems.

    Unfortunately, there are no trig functions available for the ADAU145x/6x processors. The core is pretty specialized and can't really handle them.

    Ken

  • Hi Ken,

    There's nothing to confuse. OUT2(4,5) is externally looped back to IN2(36,37).  if you refer to project file IN2 is routed to OUT3(8,9) internally. I expect to see OUT2(1Khz Sinewave) signal at  OUT3 because of external loop and internal routing. 

    Simply OUT2>IN2>OUT3.  I don't realize why this configuration will cause problems, because I'm using this configuration at 48Kz and it is working without any problem. Problem related with 192Khz sampling rate and may be related with codec. That's why I need your support. I have included project file, codec setting and block diagram that you need.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.