SIgma Studio Filter

Dear Team,

Can Someone please explain and clarify the following points for the General Filter Second Order Double Precision:

1. For a Bandpass Filter 

a. Ideally a Band pass Filter has two cut-off frequencies which is not evident in the Sigma Studio's GUI for a bandpass filter. The Filter Frequency of the BandPass filter in Sigma Studio (say i set it to 100Hz) is that the cut-off frequency ? If yes how do I interpret the single cut-off frequency for a Bandpass Filter 

b. Next what is the bandwidth in octaves and how do Interpret the range please explain with example (say for instance setting the octave to 0.90 for a 100kHz cut-off frequency) .

Regards

Hermione

Parents
  • +1
    •  Super User 
    on Aug 18, 2020 12:07 AM 3 months ago

         Hello Hermione,

         You can set the 2nd Order Bandpass filter's low and high cutoff frequencies by adjusting its two GUI settings.  The box labeled Freq is the filter's center frequency.  The -3 dB Low and High Cutoff frequencies are located at equal distances away from the center frequency when viewed on a log frequency scale.  The Bandwidth (octaves) adjustment determines the distance between these and the center frequency.

         

         For example, the bottom filter in this image has a BW of 2 octaves.  Each octave is a doubling of frequency, so two octaves means that the high cutoff frequency H must be four times more than the low cutoff frequency L.  Thus, the blue curve on the graph shows L at 50 Hz, H at 200 Hz, and the center frequency at 100 Hz.  The green and red lines correspond to filters of narrower bandwidths, as shown in this table:

         BW   Line color   Low cutoff   High cutoff

         0.5       red              84 Hz           119 Hz

         1.0     green           71 Hz            141 Hz

         2.0      blue            50 Hz            200 Hz

    In general, if we call C the center frequency, L the low cutoff, H the high cutoff, and BW the bandwidth in octaves, then:

    H = C * (2^(BW/2))    and    L = C / (2^(BW/2))

    We can work this backwards.  Given the desired cutoff frequencies L and H, the two figures to enter into the 2nd Order Bandpass Filter GUI are:

    C =  sqrt (H*L)    and      BW = 3.322 * log (H / L)

         Best regards,

         Bob

Reply
  • +1
    •  Super User 
    on Aug 18, 2020 12:07 AM 3 months ago

         Hello Hermione,

         You can set the 2nd Order Bandpass filter's low and high cutoff frequencies by adjusting its two GUI settings.  The box labeled Freq is the filter's center frequency.  The -3 dB Low and High Cutoff frequencies are located at equal distances away from the center frequency when viewed on a log frequency scale.  The Bandwidth (octaves) adjustment determines the distance between these and the center frequency.

         

         For example, the bottom filter in this image has a BW of 2 octaves.  Each octave is a doubling of frequency, so two octaves means that the high cutoff frequency H must be four times more than the low cutoff frequency L.  Thus, the blue curve on the graph shows L at 50 Hz, H at 200 Hz, and the center frequency at 100 Hz.  The green and red lines correspond to filters of narrower bandwidths, as shown in this table:

         BW   Line color   Low cutoff   High cutoff

         0.5       red              84 Hz           119 Hz

         1.0     green           71 Hz            141 Hz

         2.0      blue            50 Hz            200 Hz

    In general, if we call C the center frequency, L the low cutoff, H the high cutoff, and BW the bandwidth in octaves, then:

    H = C * (2^(BW/2))    and    L = C / (2^(BW/2))

    We can work this backwards.  Given the desired cutoff frequencies L and H, the two figures to enter into the 2nd Order Bandpass Filter GUI are:

    C =  sqrt (H*L)    and      BW = 3.322 * log (H / L)

         Best regards,

         Bob

Children