ADAU1466
Recommended for New Designs
The ADAU1462/ADAU1466 are automotive qualified audio processors that far exceed the digital signal processing capabilities of earlier SigmaDSP® devices...
Datasheet
ADAU1466 on Analog.com
Hello,
I am trying to step through a series of filters with lookup. Not too ambitious for a first SigmaStudio project I thought. But whatever setup I try, (updown LUT, pulsecount), I only get the first or the last filter index, never one in between. I use 4.5 on the 1466EVAL Some pointers in the right direction would be appreciated
Paul
Hello Paul,
You have a great start here! You got very close to a working schematic. There are just two small details I would like to point out:
With that in mind, here is a revised schematic. The readbacks are really useful for debugging this sort of thing.
The One Shot Rise w/Reset ensures that we only toggle the Pulse Counter once per cycle. We can see this on the readback. The level detector is a quick and dirty way for us to tell which filter is selected. With this setup, the level detector jumps up by 5dB once per second, so we know the proper filter is being selected.

I am attaching the project.
I hope this is helpful. Please reply if you have any further questions.
Joshua
This is very helpfull Joshua, thanks!. I would not have been able to deduct that from the wiki help.
In my system I want to write a pulse train from a raspberry to the DSP. Different number of pulses to identify a different sound index. Now the program works thanks to your input, but when I add a GPIO as input instead of the pulse source, the DSP does not respond.
I use the 1466EVAL board which has MP13 available. I set the GPIO register for that pin, basially no changes to the defaults except turning on the MP13 ( it indeed writes a 1 to the LSB of that register which fits the datasheet). And I put the i2S with which this pin is shared to slave, else I had the LRClock on the pin as well.
As first test I applied a pulse from a capacitive switch which produces a clean "pulse", no debounce needed. But the DSP does not respond. Again sort of stuck. I tried looking at the signal with the "real time display" connected to the GPIO, but nothing. Tried different number formats as well. Any new pointers perhaps?
Paul
Hi Paul,
Since you mentioned that LRCLK was still appearing on the pin after you set the GPIO register, I suspect there is something suspicious about the pin configuration. The LRCLK signal should have disappeared as soon as the pin control register was set.
Does your pin configuration look like this? The "Enable MP function of the pin" setting should be set to MP function.

If your schematic still doesn't work, can you zip it up and attach it to your response so I can take a look?
Joshua
Hi Joshua,
It also puzzled me that had to go into the serial port register as well. I am not at the same computer now so I can not check the exact settings, but I used the default. Do you also use the 1466? I remember that the enable MP was not the last field but separate red/green buttons below all the 13 port settings.
Paul
And another thought - is it actually possible to write the index number to the MP pin and connect that to the filter index directly? What would be the format? That way I can select the filter index directly on the pi instead of having to step through all filters during selection (because pulsecount would be sequential)?
Paul
Hello Paul,
If you look at the parameter list. You will see that Pulsecount does show up as a parameter. This can be read by your controller or your controller can write in a new value. This will immediately update the counter. You can actually do this right from SigmaStudio by clicking on one of the number fields and typing in a new value. This is exactly how your controller would do it.

Dave T
Hi Paul,
I am also using ADAU1466. The MP page has two sections where MP13 appears. I am highlighting them in green.
When the Mode Setting for MP13 is "Input from Pin", the output toggle button should have no effect. And when the Enable MP Function of the pin is set to "MP Function", LRCLK should disappear from the pin.

Are you able to duplicate these results?
Joshua
Hi Paul,
I am also using ADAU1466. The MP page has two sections where MP13 appears. I am highlighting them in green.
When the Mode Setting for MP13 is "Input from Pin", the output toggle button should have no effect. And when the Enable MP Function of the pin is set to "MP Function", LRCLK should disappear from the pin.

Are you able to duplicate these results?
Joshua
Hi Joshua,
For some reason I overlooked the meaning of the text.. Selected and now it works. Wonderful!