Hello all,
Following my last post:
https://ez.analog.com/dsp/sigmadsp/f/q-a/164350/adau1401a---connecting-external-slave-mode-codecs
.
[edited by: Nir76 at 11:14 AM (GMT 0) on 2 May 2020]
Hello all,
Following my last post:
https://ez.analog.com/dsp/sigmadsp/f/q-a/164350/adau1401a---connecting-external-slave-mode-codecs
Hello Nir,
1) I do not have that information and it would be very difficult to try to find this information this long after the part was designed.
2) The input capacitance of the digital pins is in the…
Hi Dave,
I did some actual measurements and you are right - the clock pins can handle a fanout of four part (including the ADAU1701 itself).
When the ADAU1701 BCLK is not connected to any load, the waveform…
Hello Nir,
You may be able to power down some of these sections if you are also not using the AUXADCs. But to be safe I would put these components into the design and don't populate them later if they…
Hello,
First of all, I know it is not a good habit to recover a resolved topic from 2 years ago, but I have almost the same problem as Nir76 . My design has a ADAU1701 and I want to drive two external audio ADCs. I was searching and found this topic. I would like to know if the resistances at the star connections are needed - and, if so, what are the recommended values.
I invoque also DaveThib because of his good answers on these chips topics.
Thanks in advance. Best regards,
Manuel
ManuelGomezOptimus Having just been through this on a design: For I2S connections, unless the traces are short, it's a good idea to always put in series termination resistors up close to the driving end. If not for good edges it also may be factor in getting your product to pass EMI testing. For whatever reason I2S signals seems to end up behind a lot of EMI issues. The exception would be if the traces are short but there I suggest at least including the series R until you can prove that removing them won't cause problems for either signal integrity nor EMI.
As to one R per fan out connection, from my experience and reading what other do that seems like the best approach. Though if driving long traces across some very large board buffering would be preferred approach.
Hi Brewster,
Many thanks for your detailed answer, I have the ideas clearer now.
BR,
Manuel
Hi Brewster,
Many thanks for your detailed answer, I have the ideas clearer now.
BR,
Manuel