Hello all,
Following my last post:
https://ez.analog.com/dsp/sigmadsp/f/q-a/164350/adau1401a---connecting-external-slave-mode-codecs
.
[edited by: Nir76 at 11:14 AM (GMT 0) on 2 May 2020]
Hello all,
Following my last post:
https://ez.analog.com/dsp/sigmadsp/f/q-a/164350/adau1401a---connecting-external-slave-mode-codecs
Hello Nir,
1) I do not have that information and it would be very difficult to try to find this information this long after the part was designed.
2) The input capacitance of the digital pins is in the…
Hi Dave,
I did some actual measurements and you are right - the clock pins can handle a fanout of four part (including the ADAU1701 itself).
When the ADAU1701 BCLK is not connected to any load, the waveform…
Hello Nir,
You may be able to power down some of these sections if you are also not using the AUXADCs. But to be safe I would put these components into the design and don't populate them later if they…
Hello Nir,
1) I do not have that information and it would be very difficult to try to find this information this long after the part was designed.
2) The input capacitance of the digital pins is in the datasheet. 5pf max. So that is some information. Often we have iBIS models for our parts but this part was designed and released before we started having the iBIS models made. So I am afraid I am not of much help here.
It is not likely you will be damaging any of the BCLK or LRCLK pins, since you are not trying to drive a short and most parts can handle a fanout of more than three. If you look at the scope and see that it is not able to drive the load with your test then I would be concerned. Your test is sort of a worst case with no damping resistors so if there is too much capacitance your rise time will be slow. If your test looks good then I think you are fine since your design will end up with some damping resistors.
Look at the scope and run the system at the highest sample rate you will be using and then see what the timing margin is between the BCLK and SDATA. That will be another good test.
Dave T
Hi Dave,
I did some actual measurements and you are right - the clock pins can handle a fanout of four part (including the ADAU1701 itself).
When the ADAU1701 BCLK is not connected to any load, the waveform looks like this: (Using an active probe with 1pF capacitance)
The BCLK is 3.072MHz, rise and fall time are about 6nsec, the signal BW is about 0.35/6nsec = 58MHz
When the ADAU1701 BCLK is connected to four loads, the waveform looks like this:
In this condition, rise and fall time are about 14nsec. the signal BW was reduced to about 0.35/14nsec = 25MHz
Still, 25MHz of BW can transfer 5 harmonics of the clock square wave...
The signal looks clean, no over/undershoots. the extra capacitance did caused the rise/fall time to increase, but this is understandable.
I remind you that this measurement is with no termination resistors or solid ground plane underneath the signal, so in the final PCB things should even get better.
Thanks again for your kind help.
Nir
Hello Nir,
These signals look really good so that is good news. You should be able to proceed with your tests
Dave T
Hi Dave,
Thanks for replying to my last posts!
In order complete the hardware design, I have another question regarding not connected pins.
In my design, I'm using only the digital ports, no ADCs or DACs
Can I leave all the ADC/DAC pin unconnected?
I'm referring to these pins:
1- ADC0,1
2- VOUT0,1,2,3
3- FILTA, FILTD
5- ADC_RES
6- CM
Thanks again!
Best Regards,
Nir
Hello Nir,
You may be able to power down some of these sections if you are also not using the AUXADCs. But to be safe I would put these components into the design and don't populate them later if they are not needed.
The FiltA, FiltD and the CM pins you still should bypass to keep the references from oscillating and causing problems in the part.
You should include the ADC_RES for the same reason.
The ADC in is a good idea to cap couple to ground. You can directly ground it but it will draw some current due to the CM bias. You do not need a huge cap. 10uf will be great but you could probably get away with 4.7uf or 2.2uf.
The DAC outputs can be left floating. If you feel you have to terminate them then use a 10K to ground.
Then experiment with the board. Shut off power to the ADCs and DACs and shut off the internal reference supply. Then see if the part works and there is no voltage on the CM and FILTx pins. What I am concerned about is that some of these older parts had some strange "bugs" in that shutting down some sections of the parts would cause other sections not to function. So this is why I am saying to design in the parts then experiment with it afterwards if possible.
I could experiment here if I have time but that might not be for a while,
Dave T
Hello,
First of all, I know it is not a good habit to recover a resolved topic from 2 years ago, but I have almost the same problem as Nir76 . My design has a ADAU1701 and I want to drive two external audio ADCs. I was searching and found this topic. I would like to know if the resistances at the star connections are needed - and, if so, what are the recommended values.
I invoque also DaveThib because of his good answers on these chips topics.
Thanks in advance. Best regards,
Manuel
ManuelGomezOptimus Having just been through this on a design: For I2S connections, unless the traces are short, it's a good idea to always put in series termination resistors up close to the driving end. If not for good edges it also may be factor in getting your product to pass EMI testing. For whatever reason I2S signals seems to end up behind a lot of EMI issues. The exception would be if the traces are short but there I suggest at least including the series R until you can prove that removing them won't cause problems for either signal integrity nor EMI.
As to one R per fan out connection, from my experience and reading what other do that seems like the best approach. Though if driving long traces across some very large board buffering would be preferred approach.
Hi Brewster,
Many thanks for your detailed answer, I have the ideas clearer now.
BR,
Manuel