Bug in Voltage Controlled (Fractional) Delay Block???

I'm seeing some unexpected behavior with the voltage-controlled fractional delay block in SigmaStudio. The processor I'm using is the ADAU1466 with a sample rate of 48kHz. The maximum delay in the block is 36000 samples (750ms at 48kHz).

When setting the input voltage to 0V using a DC source, I'm seeing a delay of roughly 615ms (should be 0ms). When setting the input voltage to 0.0625V (1/16V step size), I'm seeing a delay of roughly 662ms (should be 46.875ms) . Larger step sizes produce the expected delay. For example, 0.125V input produces 93.75ms delay, 0.250V input produces 187.5ms delay and so forth.

Can anyone else confirm this?

Thanks,
Larry Y.