Post Go back to editing

ADAU1466 strange problem with SPDIF -ASRC - two boards linking

Hello to All

We use  ADAU1466 on our own developped board   ( hifi product ).   .  Clock at 12.288 Mhz  -   Everything is working fine until now

Our program  is including  serial IN ( from ADC)  and  SPDIF input through ASRC . To make it short, these inputs are sent to serial out ( dac )  and spdif out (  from DSP)  .    The goal is to link several dsp board via SPDIF  input-output . ( DSP is making some instructions  before to output the SPDIF  and before SERIAL output, thus we can not use the simple redirection option in routing matrix) 

When we send a  signal (from 1st board )  in the SPDIF input (2nd board)   using this basic  program  , SPDIF INPUT  locking is correct and  output signal from DAC is stable .

But when we add some more instructions into this program,  SPDIF INPUT locking  becomes incorrect / unstable .  ( it locks 1 or 2 seconds and lose it   and relocks and lose it etc )

Kindly note we have the same problem if we change to Fs48KHz . We tried different setting for  in the SPDIF hardware window but it didn't help .

The only way  to get the 2nd board working correctly  is to choose "spdif receiver" option into the "start pulse"  option folder .  (clock control window ) .

Thus it seems ASRC doesn't make the correct job .  ( adding few instructions into the program is making the SPDIF and /or ASRC  unstable --- a bit strange )

I hope to be clear enough in my explanations .  ( programs are attached )

Any help and suggestion will be welcome .

Thanks a lot

  • Hello TH25,

    I am looking into this... Thanks for sending the files.

    Dave T

  • Hi. Are the programs that you uploaded running on the sending board, the receiving board, or both?

    I've added a little instrumentation to your "not working" program. The left half checks the status of the Rx lock, and the right half checks the status of the Tx enable. Both seem well behaved for me. After letting it run for a while, I'm not seeing any loss of lock from an incoming S/PDIF stream or loss of the transmitter.

    Would you please add this logic and confirm that the processor thinks you are losing lock on your hardware? The new blocks are Basic DSP > Logic > Toggle > One Shot Rise and One Shot Fall.

    I did notice a separate issue with your project, though, that may or may not be related. I see that your project is set up to run at 96 kHz. The GUI is confusing, but the menu at the top only controls the graphical environment. To set the hardware to 96 kHz with a 12.288 MHz crystal, you need to change the clock divider in the CLOCK_CONTROL tab of the register window from 1/6 (48 kHz) to 2/6 or 1/3:

    You will need to fix this, regardless, since your DAC is likely zero-padding between samples and every second sample from your ADC is likely being ignored. It seems unlikely, but perhaps this is related.

    Ken

  • Dear Ken

    Thank you very much for your detailed reply and suggestion

    The program we sent are on the receiver board .  ( sender  is very simple program  with 1 asrc input and 1 spdif out  - no problem with it )

    As to the 2nd issue you found,  I think it is related to issue 1  but there is something which is not clear at all for us.

    Of course, we adjusted "clock control" parameters  according to the sampling frequency (96kHz) .  you can see screen copy here  .

    But as you can see,  if we want the signal (96kHz verified ) from SPDIF input  is correctly proceed ( correct locking ) we must set the "start pulse" to  base fs *2   .   (in base fs, locking is failing )  . But in such case, it means the core and DAC are working in 192 k .  ( since Start pulse is chosen @  *2 )

    As you can see, we read  paramater F582  (asrc ratio) and in this case , it shows 0.5

    As you can see either we included your little instrumentation .  In  2/6 with start pulse 2*fs  , there is no locking lost .  But if we chose 1*Fs instead ,  the "lock is ever lost" is showing  1 very quickly .  ( We also monitor the F600 variable  ... )

    One question by the way, you said we must choose  2/6  instead of 1/6 .  But what is the difference if we choose n/m at 1/6 , start pulse @ 2*FS  and choose the 2*Fs  option into the serial port configuration window  ?

    Thanks a lot in advance  

  • Hello Dave . Have you seen something wrong on your side ?

  • The SigmaDSP family are, for the most part, stream processors. This means that the algorithm executes completely once per sample period. If you are doing block processing, that is done in the "leftover" time. START_PULSE sets the interrupt source that tells the processor to begin computing the next sample frame. In essence, this is what sets the core's sample rate. In the majority of application, the source for START_PULSE is Base_Fs, corresponding to the rate of CLKGEN1 x1. This default setting works for most people, but not here.

    If I understand correctly, you would like to lock the entire processor to the recovered rate of the incoming S/PDIF signal. This is possible, but it takes some setup as follows:

    On the CLOCK_CONTROL tab:

        START_PULSE = S/PDIF receiver rate
        CLKGEN3 N = 1024
        CLKGEN3 SRC = Locks on FREF, needs N
        FREF source = FREF comes from S/PDIF receiver

    On the ROUTING_MATRIX tab:

        ASRC0 Source = From S/PDIF receiver
        ASRC0 Output rate = Use DSP rate
        SPDIF Tx = From DSP

    On the SPDIF tab:

        SPDIF TX EN = Enabled
        SPDIF Rx and Tx MCLKSPEED = SYSCLK
        SPDIF RESTART = Enabled (green)

    An example project with these settings is attached, but I'll walk you through.

    START_PULSE is set to the S/PDIF receiver rate forcing the core's sample rate to be equal to the recovered clock. CLKGEN3 is configured to track this same rate by way of FREF. The S/PDIF signal comes in through ASRC0. However, by setting the output rate of the ASRC to Use DSP rate, you are forcing it to track START_PULSE, which is the same rate. Therefore, the ASRC ratio is locked at 1, and it is not really doing any sample rate conversion. The S/PDIF transmitter is also set to output at the DSP rate so the Tx and Rx rate are the same. The S/PDIF transmitted must be manually enabled, and setting the MCLKSPEED to SYSCLK allows is to run up to 192 kHz if need be and gives more headroom around 96 kHz.

    The second piece of the puzzle is mixing in an I2S stream from an ADC. If the DSP is the clock master (the ADC is the clock slave), then the SPORT should be set to:

        Sampling rate = Fs
        Clock Generator = Clock generator 3
        BCLK/LRCLK source = master

    This will run the serial port at the same base Fs as the core, which is locked to the S/PDIF input rate. If the ADC needs to be a clock master, you will need to use another ASRC, but the sampling rate should still be set to Fs. If the rate is set to Fs*2, you will just be repeating samples on the output.

    Lastly, you should be aware of some idiosyncrasies of the S/PDIF receiver. The first is that the ASRC outputs a DC value until it is able to lock on the input clock. It is a very good idea to check the lock status bit manually and mute when it is not locked. I've included an example showing this, as well. It's written for the ADAU1452, but it works identically.

    Ken

    ADAU1466-Lock-All-to-SPDIF-Input.zip

    ADAU1452-ASRC-Lock-Detect-Example.zip 

  • Dear Ken

    Thanks a lot for your detailed answer.

    If I understand correctly, you would like to lock the entire processor to the recovered rate of the incoming S/PDIF signal. This is possible, but it takes some setup as follows:

    No ,  we don't want this .

    My explanation is certainly badly conveyed. I am sorry .  Actually,   we don't want to lock the core according the spdif input ........  I just said if we use this option into the program I attached previously  , we succeed to get a stable signal from spdif  . Just try to give you some more information on what we tested .   But so far , we want to use regular way  with core timing reference ..... Thus using ASRC for it normal job !  and this is where we have problem ... :-(

    Th.

  • OK. Please list all of the inputs and outputs, the sample rate for each, and which are clock master/slave. I'll walk you through setup.

    Ken

  • In order to avoid any problem we setup the  GEN1 to  2/6 as you said.   Start pulse to BASE FS  

    The serial input and ouput ports  are set on BASE FS   and CLOCK GEN1

    We have SPDIF input    (we can provide signal in  it  at 96 kHz or 48 or 44  ) .

    ASRC 0 is set to SPDIF receiver  ( and use DSP rate)

    We have no problem for analog in .  ADC  , DSP and DAC are working correctly

    We have problem with SPDIF input .  It seems the ASRC is not doing it job correctly   when program is medium to bi sized .  ( if program is very small , it works and this where it is strange )

  • If I insert this into your project above called test-spdif-notworking,dsproj, it correctly reads 1 when I give it 96 kHz over S/PDIF and 0.5 when I give it 48 kHz. Is it doing this on your hardware?

        

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.