[Bug Report] Parameters of ADAU1452 AVC exported twice

Title: Parameters of ADAU1452 AVC exported twice

Description: When an ADI Algorithms->AVC->Automatic Volume Control block is used for an ADAU1452, its parameters are exported twice. That means the XML file and the C header each contain two entries per address. The entries have the same content (address, value).

<ModuleParameter>
    <Name>TV_AVCassembly145X1Decay</Name>
    [..]
</ModuleParameter>
<ModuleParameter>
    <Name>TV_AVCassembly145X1Decay</Name>
    [..]
</ModuleParameter>

#define MOD_AUTOMATICVOLUMECONTROL1_ALG0_TVAVCASSEMBLY145X1DECAY_ADDR 30
#define MOD_AUTOMATICVOLUMECONTROL1_ALG0_TVAVCASSEMBLY145X1DECAY_VALUE SIGMASTUDIOTYPE_8_24_CONVERT(1.66666666666667E-05)
#define MOD_AUTOMATICVOLUMECONTROL1_ALG0_TVAVCASSEMBLY145X1DECAY_TYPE SIGMASTUDIOTYPE_8_24
#define MOD_AUTOMATICVOLUMECONTROL1_ALG0_TVAVCASSEMBLY145X1DECAY_ADDR 30
#define MOD_AUTOMATICVOLUMECONTROL1_ALG0_TVAVCASSEMBLY145X1DECAY_VALUE SIGMASTUDIOTYPE_8_24_CONVERT(1.66666666666667E-05)
#define MOD_AUTOMATICVOLUMECONTROL1_ALG0_TVAVCASSEMBLY145X1DECAY_TYPE SIGMASTUDIOTYPE_8_24

The attachment contains an example project and the exported XML and C header files: SigmaStudio_AVC_parameter.zip


SigmaStudio Version: 4.2. Build 1, Rev. 1764

OS: Windows 7 64Bit, Service Pack 1