The context is:
Custom board designed to be modular --- each particular board will use either L, or R, or possibly both, and may work with a particular audio band or with the full spectrum.
Thus, I want to output the entire audio input ("entire" as in: both channels, full bandwidth --- simply put: an exact copy of the input) so that the next modules (the next boards) can use any portions of the audio as they need.
EDIT: Forgot to mention: the reason why I don't simply have each board "tap" into a master/broadcast I2S set of signals is that one of the modules may actually get audio from the DACs; then, that module would output the audio through I2S for the rest of the modules to work with it.
For the ADAU1701 in SigmaStudio, I understand that ports 2 and 3 of an Input control map to L and R (respectively) of the first I2S input --- correct? (the documentation says "first channel in I2S or TDM stream" --- not 100% sure what "first channel" means). And Dig0 and Dig1 map to L and R of the first I2S output (SDATA_OUT0).
Is it just a matter of connecting port 2 of the input to a Dig0 output control, and port 3 to Dig1 ? (see example in the figure below, where the module would implement a 2-way crossover for the left channel, so that presumably a second module would do the same for the right channel)
Any special configuration needed?
Thanks,
Carlos
--
Clarification added
[edited by: cmoreno_uw at 8:57 PM (GMT 0) on 25 Jan 2019]