[Bug Report] Export file contains addresses of second DSP

Title: Export file contains addresses of second DSP

Description: The project contains two DSPs, ADAU1442 (IC1) and ADAU1452 (IC2). After a "Link Compile Download" and Export, the generated parameter XML file contains entries of IC1 in the IC2 section. For example address 57888 (0xE220) is included for both ICs with the name "IC 1.Start_Pulse_Select". This was not the case when using Sigma Studio 4.1. Furthermore I cannot find the address in the data sheet of IC2.

To sum up:

  1. Why does the IC2 section of the XML file contain an entry with the name "IC 1...."?
  2. The data sheet of DSP1452 (IC2) ("SigmaDSP Digital Audio Processor, ADAU1452/ADAU1451/ADAU1450" Rev C) does not contain the address in the memory map. Why is there an address in the parameter file that is not described in the data sheet?

SigmaStudio Version: 4.2. Build 1, Rev. 1764

OS: Windows 7 64Bit, Service Pack 1

Parents Reply Children