hello I need an echo effect how do I make something like this thank you
ADAU1701
Production
The ADAU1701 is a complete single-chip audio system with a 28-/56-bit audio DSP, ADCs, DACs, and microcontroller-like control interfaces. Signal processing...
Datasheet
ADAU1701 on Analog.com
hello I need an echo effect how do I make something like this thank you
Hello,
adau1701 isn't really suited for echo/delay effects unless you are happy with very short delay times...You can get a maximum of 42ms at 48khz, actually less because each other block in your project will take up some memory too.
There's a schematic from the great KJBob which can double the delay time by using a Synchronous Multiplexer:
https://ez.analog.com/dsp/sigmadsp/f/q-a/64755/guitar-reverb-and-adau-1701/451610
If you need more delay time adau14xx can do that.
maybe you have a recommendation for me for a dsb board
Hello ,
ADAU1452Z Rev.B would be a good choice.
You can go with either ADAU145x or ADAU146x series Eval boards. The ADAU146x series have higher memory unit.
Regards
Harish