hello can someone help me and i would like a 3 band EQ and a volume turner and that on the potentiometer of the wondom dsp would be happy for help i just can't do it
ADAU1701
Production
The ADAU1701 is a complete single-chip audio system with a 28-/56-bit audio DSP, ADCs, DACs, and microcontroller-like control interfaces. Signal processing...
Datasheet
ADAU1701 on Analog.com
hello can someone help me and i would like a 3 band EQ and a volume turner and that on the potentiometer of the wondom dsp would be happy for help i just can't do it
Hello Lorenzo,
My eval board has only one pot so i made an example volume control and a separate one-band EQ. Please download and open them to observe how they're built. You'll need to build up your circuit by cascading the volume control and three EQs, setting them to the desired frequencies. Use one Aux ADC with one pot on your Wondom board to control each of these. Set the HW Config / Register Settings to assign the MP pins for the Aux ADCs (I'm only using ADC3, which corresponds to MP8).
Best regards,
Bob