Sigma Studio Parameter Window Page Under Construction

Dear Team ,

Since the Sigma Studio, Parameter page is under Construction since time immemorial, I would like to ask you a few pertinent questions here as below:

1. The IC Params Window displays details about the Parameter Name, Address,Data for  only up to 20K memory i.e for DM0  although the Parameter RAM is 40K for ADAU1452 . How do I then access the rest 20 K which I suppose is allocated to DM1 memory .

2.Yes please do not suggest exporting the files using Link Compile Download  or looking up the Capture window instead ,since I need to access the DM1 contents / rest of the 20K Parameter RAM in the Params IC window strictly