Article SigmaStudio 3.9.2 Beta Available for Download

SigmaStudio 3.9.2 Beta Available for Download by ADIApproved

The latest SigmaStudio Beta release is available for download here: http://www.analog.com/en/dsp-software/ss_sigst_02/sw.html

You will need to log in with your MyAnalog account to access the download.

Here are a list of the updates in recent versions:

Updates SigmaStudio 3.9.2 BETA

  • Export to Linux files now supports XML format. Implementation of Export to Linux files for ADAU1701.
  • Single band level detector supports linear display.
  • New peak dynamics processors with external detect (Mono/Stereo) that supports fast release for low frequencies.

 

Updates SigmaStudio 3.9.1 BETA

  • Single band level detector has now a new graphic adjustable display.
  • Added All-pass selection to “First Order Filters” type in General (2nd Order) Filter
  • Added user selectable phase wrapped/un-wrapped and radians/degrees options in probe window

Bug Fixes SigmaStudio 3.9.1 BETA

  • FIR Filter table is fixed, with all coefficients set to zero except the first.

 

Updates SigmaStudio 3.9.0 BETA

  • Extended probe window frequency axis to 96kHz maximum.
  • Added log lookup table for ADAU170x and ADAU144x.
  • Made simple sub-harmonic support ADAU176x, ADAU1781 and ADAU144x.
  • Added Quad VCO support ADAU1701 and AD1940.
  • Added VCO with flexible phase for ADAU170x and ADAU144x.
  • Added two externally triggered sweeps for ADAU170x and ADAU144x.
  • Added square root approximation for ADAU170x and ADAU144x.
  • Added peak compressor with zero cross for ADAU176x, ADAU1781 and ADAU144x.
  • Added elliptical interpolated IIR low pass filter for ADAU176x, ADAU1781 and ADAU144X.

Bug Fixes SigmaStudio 3.9.0 BETA

  • Change schematic view mouse wheel zoom steps to match the zoom menu zoom step sizes.
  • Decrease font size and add tooltips in the ADAU144X register window to fix readability issues.
  • Optimized schematic linking reduces compile times for large projects


RE: SigmaStudio 3.9.2 Beta Available for Download by KJBob:

     Hello Brett,

     In addition to the new features you listed, it appears that SigmaStudio 3.92 fixes the alias bug reported at:

https://ez.analog.com/message/89632#89632

     Thanks to you, Miguel, and the SigmaStudio team!

     Best regards,

     Bob


RE: SigmaStudio 3.9.2 Beta Available for Download by ADIApproved:

Thanks for pointing this out, Bob!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.