Article New SigmaStudio 3.3 Beta Version Available

New SigmaStudio 3.3 Beta Version Available by JeradL

There is a new beta, version 3.2, of SigmaStudio available on the software's download page. The most significant update included in this version is support for both the Windows 7 OS and x64 (Vista and 7) processors. This version should not be used for production designs, but rather to preview bug fixes and new features that will be available in the next release. Please feel free to download this version and report any bugs (or things you like!) in the thread below. The download file includes installers for both x86 (32-bit) and x64 (64-bit) versions; please choose the appropriate one for your PC.

The release information for this version includes:

Enhancements in SigmaStudio 3.3.0

  • Windows      Vista and Windows 7 x64 support.
  • New      installation process:
    • Default       Installation file path location for x64 architecture is Program Files       (x64).
    • Default       SigmaStudio projects path location is \<users>\Documents\Analog       Devices\SigmaStudio\Projects.
    • During       installation process, the user will be prompted with an additional USBi       installation. This is to install the right USBi drivers into the current       machine and it only needs to be run once.
  • PLL      wait command during “download-compile”.
  • Export      uC files with the wait command. This includes Sequencer support on wait      command.
  • Envelope      time span from 10 ms to 4400 ms.
  • Peaking      No Post Gain now supports full range.


RE: New SigmaStudio 3.3 Beta Version Available by JeradL:

Note that in order to install SigmaStudio, you should double-click on the setup.exe file in the .zip download, not Sigma Studio.msi.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.