My microcontroller does not have a C compiler. How do I use a microcontroller to boot my SigmaDSP in assembly?
_________________________________________________________________
In SigmaStudio, a number…
Recently there have been some email support requests regarding the calculation of filter coefficients (and other types of parameters) for storage in a microcontroller. The basic idea is to store a table…
Question: Can I program multiple SigmaDSPs in parallel using one USBi?
Answer: Yes, you can string together multiple SigmaDSPs on one or more PCBs and control them with a single USBi.
If all of the…
Question:
I have read through SigmaDSP datasheet, and I find no related information on the MP3/WAV/AAC decoding engine for SigmaDSP.
Is there any available audio decoder for SigmaDSP like those modules…
There is not a C compiler for SigmaDSP, and we do not support custom assembly coding in SigmaStudio. The built-in library includes many different signal processing blocks. Low-level blocks, such as multipliers…
The SigmaDSP processors up to the current generation do stream-oriented processing, otherwise known as sample-by-sample processing. This means that a sample is input and output at a rate equal to the sample…
No, the SigmaStudio software is licensed for use as a design tool and is not intended for use as a mass-market tuning/programming tool. If your product design requires a software interface for tuning audio…
Creating a delay after startup by BrettG
If a delay is required after starting up the SigmaDSP and before audio starts outputting, a stopwatch cell can be used. An example project is attached.
For…
Hi everybody,
I thought I would contribute to the selection of FAQs on EngineerZone by writing up a short summary of a question that is often asked on the forums.
Q: For my audio application, I intend…
It's pretty easy to use SigmaStudio to build your signal flow and output the utilized resources. Every time you compile a project, a file called compiler_output.txt is generated in the folder in which…