Locale Icon
English
EngineerZone
EngineerZone
SHARC Processors
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
    Power Management Fundamentals II Session 6: Key Layout Considerations for Power

    Understand the physics of printed circuit boards to manage large changes in current or voltage. See how layout tweaks can make big improvements for your...
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
    • Enabling New Space Missions: ADI’s Commercial Space Screening Approach for Agile, High-Reliability Payloads
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3

    Noise analysis of a circuit requires tracking several things simultaneously: each noise source, how those noise sources are shaped by the circuit, and...

     

    ​​Where Errors Lurk in the GMSL Signal Chain​

    Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...

    Latest Blogs

    • Achieving Power Over Data with RS-485 Transceivers
    • ​​Functional Safety: A Driver of “Shift Left”​
    • The 5 Advantages of Hardware Fault Tolerance
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
SHARC Processors
  • Processors & DSP
SHARC Processors
Documents Output L and R channels are reversed in AD1939_I2S_Sampled_Based_Talkthru BSP code for ADSP-21469
  • Forums
  • Documents
  • Members
  • Tags
  • Cancel
  • Documents
  • +214xx IIR AcceleratorL FAQ
  • +214xx processors: FAQ
  • Accessing SPI Flash with more than 128Mb *LDR
  • +ADSP-21364: FAQ
  • +ADSP-21369: FAQ
  • +ADSP-21371: FAQ
  • +ADSP-21469: FAQ
  • +ADSP-21479: FAQ
  • +ADSP-21489: FAQ
  • +ADSP-2148x: FAQ
  • +ADSP-SC58x: FAQ
  • ADSP-SC594 - DDR Sweep Test
  • +ADSP-SC5xx/215xx Boot with CRC32
  • +ADSP-SC83x/ADSP-2183x
  • +Breakpoint: FAQ
  • +Debug an Application: FAQ
  • Do we need to use Static Voltage Scaling (SVS) to operate the ADSP-2148x in 450MHz?
  • Does ASRC TDM mode used the opposite clock edge as in other modes such as I2S for sampling and driving the inputs and outputs?
  • elfloader Commands for Generating an ADSP-SC594 single and Multicore Loader Stream.
  • Example commands for generating Secure loader streams for SC59x and 2159x processors
  • Example for FIR Decimation and Interpolation Sampling using ADSP-21569
  • Example for Octal SSL Booting using SC594
  • Example for SPI Slave Boot mode for ADSP-21489 using CCES
  • Example to issue a system reset when watchdog expiration event occurs
  • Features of OTP over Secure Booting
  • FIR Accelerator performance degrades when modifier(ADI_FIR_CHANNEL_INFO structure) are other than 1
  • How to configure DAI pins as GPIO?
  • How to enable all the SPORTs (0-7) at the same time in ADSP-SC59x/ADSP-2159x?
  • How to program the system core FLAG pins in ADSP-2156x
  • How to properly invalidate the Pre-Fetch Buffer?
  • How to read the status of SYS_BMODE pins using software for ADSP-21569 and ADSP-21593?
  • How to select PCG Input source for ADSP-SC59x
  • +I2S PCG: FAQ
  • Is it feasible to transition the pins mode from SPI functionality to GPIO after booting the DSP from SPI master?
  • Is it possible to boot the program code from HyperFlash and execute it in HyperRAM?
  • Is it possible to recover the information from Loader(LDR) or executable(DXE) files.
  • Is it possible to use the ADSP-21569 init code for ADSP-21565?
  • Is it possible to use the same pin as SPI_SS as a GPIO interrupt trigger when using SPI simultaneously?
  • +JTAG: FAQ
  • MTM DMA transfer on ADSP-21489
  • Output L and R channels are reversed in AD1939_I2S_Sampled_Based_Talkthru BSP code for ADSP-21469
  • Pre-boot time for ADSP-2156x and ADSP-SC59x/ADSP-2159x
  • Second stage loader example for SC594
  • +SHARC family: FAQ
  • +SHARC processor: FAQ
  • SPI Chain DMA example for ADSP-21489
  • SPI example for ADSP-21369
  • SPI Master to Slave loopback communication in ADSP-21569
  • +SPI serial flash driver: FAQ
  • SSL example for ADSP-21593
  • +SSL: FAQ
  • Support for Automatic Device Detection in Secure Booting
  • Tiny Cache in ADSP-2156x and ADSP-SC59x/ADSP-2159x
  • +USB VID/PID: FAQ
  • Value of DDR reference resistor (DMC0_RZQ) and ZQ for SC594
  • What is the behavior of Circular Buffer mode?
  • What is the difference between “adi_signtool.exe” and “signtool.exe”? Does “adi_signtool.exe” only be used with GLXP?
  • What is the effect of enabling/disabling the ADI_SPORT_BLOCKING_MODE
  • What is the maximum supported clock frequency in Linkport DDR mode for SC594
  • What is the priority of programmable interrupts in comparison to core software interrupts (SFT0I–SFT3I)?
  • What is the Reset value of PADS_PCFG.FAULT_DIS bit ADSP-2159x and SC59x processors
  • What is the SPU_ID for EMDMA0/1 channels in ADSP-SC594/21594
  • Where can I find the 2Mbits memory map configuration for ADSP-21488 automotive parts?
  • Why does the UART TX interrupt trigger before THR and TSR are empty?
  • Why is it mandatory to send 1024-byte blocks during Secure SPI slave boot?

Output L and R channels are reversed in AD1939_I2S_Sampled_Based_Talkthru BSP code for ADSP-21469

Revision Creation Date Revision Author
Current Revision 31 Mar 2023 2:18 AM Divya.P
  • View current version