Locale Icon
English
EngineerZone
EngineerZone
SHARC Processors
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
    Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers
    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers

    Introduction to Industrial I/O, libIIO, and Python software tools

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

SHARC Processors
  • Processors & DSP
SHARC Processors
Documents Second stage loader example for SC594
  • Forums
  • Documents
  • Members
  • Tags
  • Cancel
  • Documents
  • +214xx IIR AcceleratorL FAQ
  • +214xx processors: FAQ
  • Accessing SPI Flash with more than 128Mb *LDR
  • +ADSP-21364: FAQ
  • +ADSP-21369: FAQ
  • +ADSP-21371: FAQ
  • +ADSP-21469: FAQ
  • +ADSP-21479: FAQ
  • +ADSP-21489: FAQ
  • +ADSP-2148x: FAQ
  • +ADSP-SC58x: FAQ
  • ADSP-SC594 - DDR Sweep Test
  • +ADSP-SC5xx/215xx Boot with CRC32
  • +ADSP-SC83x/ADSP-2183x
  • +Breakpoint: FAQ
  • +Debug an Application: FAQ
  • Do we need to use Static Voltage Scaling (SVS) to operate the ADSP-2148x in 450MHz?
  • Does ASRC TDM mode used the opposite clock edge as in other modes such as I2S for sampling and driving the inputs and outputs?
  • elfloader Commands for Generating an ADSP-SC594 single and Multicore Loader Stream.
  • Example commands for generating Secure loader streams for SC59x and 2159x processors
  • Example for FIR Decimation and Interpolation Sampling using ADSP-21569
  • Example for Octal SSL Booting using SC594
  • Example for SPI Slave Boot mode for ADSP-21489 using CCES
  • Example to issue a system reset when watchdog expiration event occurs
  • FAQ: What happens when the IMDW0 bit is changed, and why does the same address behave differently for 32-bit and 40-bit accesses?
  • Features of OTP over Secure Booting
  • FIR Accelerator performance degrades when modifier(ADI_FIR_CHANNEL_INFO structure) are other than 1
  • How to configure DAI pins as GPIO?
  • How to enable all the SPORTs (0-7) at the same time in ADSP-SC59x/ADSP-2159x?
  • How to program the system core FLAG pins in ADSP-2156x
  • How to properly invalidate the Pre-Fetch Buffer?
  • How to read the status of SYS_BMODE pins using software for ADSP-21569 and ADSP-21593?
  • How to select PCG Input source for ADSP-SC59x
  • +I2S PCG: FAQ
  • Is it feasible to transition the pins mode from SPI functionality to GPIO after booting the DSP from SPI master?
  • Is it possible to boot the program code from HyperFlash and execute it in HyperRAM?
  • Is it possible to recover the information from Loader(LDR) or executable(DXE) files.
  • Is it possible to use the ADSP-21569 init code for ADSP-21565?
  • Is it possible to use the same pin as SPI_SS as a GPIO interrupt trigger when using SPI simultaneously?
  • Is the "double" datatype 32-bit or 64-bit on SHARC?
  • +JTAG: FAQ
  • MTM DMA transfer on ADSP-21489
  • Output L and R channels are reversed in AD1939_I2S_Sampled_Based_Talkthru BSP code for ADSP-21469
  • Pre-boot time for ADSP-2156x and ADSP-SC59x/ADSP-2159x
  • Second stage loader example for SC594
  • +SHARC family: FAQ
  • +SHARC processor: FAQ
  • SPI Chain DMA example for ADSP-21489
  • SPI example for ADSP-21369
  • SPI Master to Slave loopback communication in ADSP-21569
  • +SPI serial flash driver: FAQ
  • SSL example for ADSP-21593
  • +SSL: FAQ
  • Support for Automatic Device Detection in Secure Booting
  • Tiny Cache in ADSP-2156x and ADSP-SC59x/ADSP-2159x
  • +USB VID/PID: FAQ
  • Value of DDR reference resistor (DMC0_RZQ) and ZQ for SC594
  • What is the behavior of Circular Buffer mode?
  • What is the difference between “adi_signtool.exe” and “signtool.exe”? Does “adi_signtool.exe” only be used with GLXP?
  • What is the effect of enabling/disabling the ADI_SPORT_BLOCKING_MODE
  • What is the maximum supported clock frequency in Linkport DDR mode for SC594
  • What is the priority of programmable interrupts in comparison to core software interrupts (SFT0I–SFT3I)?
  • What is the Reset value of PADS_PCFG.FAULT_DIS bit ADSP-2159x and SC59x processors
  • What is the SPU_ID for EMDMA0/1 channels in ADSP-SC594/21594
  • Where can I find the 2Mbits memory map configuration for ADSP-21488 automotive parts?
  • Why does the UART TX interrupt trigger before THR and TSR are empty?
  • Why is it mandatory to send 1024-byte blocks during Secure SPI slave boot?

Second stage loader example for SC594

An SSL is a stand-alone application that is executed at boot time before the actual application is dynamically loaded into memory. The SSL can be used to invoke a ROM API to boot a second application.

The attached example code is for SSL in SC594, which boots a simple user application from ARM core using ROM api.

LEDs 2,4,5 will blink in the user Application when calling the adi_rom_boot command.
 
Using the attached Loader.bat file, loader files for SSL and User Application generated.
Using CLDP.bat file, SSL and user application loaded in different offset address of flash.  


When flash process is done, switch to boot mode 1 and reset the board.
SC594_SSL_booting.zip

  • Share
  • History
  • More