The ASRC can operate in TDM, I2S, left-justified, right-justified, and bypass modes. The serial ports of the processor can be used for moving the ASRC data to/from the internal memory. This example is used to demonstrate the ASRC in TDM8 mode. 4 ASRCs are daisy-chained together and connected to the serial port of a SHARC processor to achieve TDM8 mode of operation.