Locale Icon
English
EngineerZone
EngineerZone
SHARC Processors
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
    Power Management Fundamentals II Session 5: Deeper Look into Power Protection

    When is the best time to discover your power circuit needs protection? Let's explore the use of some input protection and control options like ideal diodes...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

     

    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

    Latest Blogs

    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
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
SHARC Processors
  • Processors & DSP
SHARC Processors
Documents Selective Booting of One Application from Multiple Applications using CCES for ADSP-21479
  • Forums
  • Documents
  • Members
  • Tags
  • Cancel
  • Documents
  • +214xx IIR AcceleratorL FAQ
  • +214xx processors: FAQ
  • Accessing SPI Flash with more than 128Mb *LDR
  • +ADSP-21364: FAQ
  • +ADSP-21369: FAQ
  • +ADSP-21371: FAQ
  • +ADSP-21469: FAQ
  • -ADSP-21479: FAQ
    • Selective Booting of One Application from Multiple Applications using CCES for ADSP-21479
  • +ADSP-21489: FAQ
  • +ADSP-2148x: FAQ
  • +ADSP-SC58x: FAQ
  • ADSP-SC594 - DDR Sweep Test
  • +ADSP-SC5xx/215xx Boot with CRC32
  • +ADSP-SC83x/ADSP-2183x
  • +Breakpoint: FAQ
  • +Debug an Application: FAQ
  • Do we need to use Static Voltage Scaling (SVS) to operate the ADSP-2148x in 450MHz?
  • Does ASRC TDM mode used the opposite clock edge as in other modes such as I2S for sampling and driving the inputs and outputs?
  • elfloader Commands for Generating an ADSP-SC594 single and Multicore Loader Stream.
  • Example commands for generating Secure loader streams for SC59x and 2159x processors
  • Example for FIR Decimation and Interpolation Sampling using ADSP-21569
  • Example for Octal SSL Booting using SC594
  • Example for SPI Slave Boot mode for ADSP-21489 using CCES
  • Example to issue a system reset when watchdog expiration event occurs
  • Features of OTP over Secure Booting
  • FIR Accelerator performance degrades when modifier(ADI_FIR_CHANNEL_INFO structure) are other than 1
  • How to configure DAI pins as GPIO?
  • How to enable all the SPORTs (0-7) at the same time in ADSP-SC59x/ADSP-2159x?
  • How to program the system core FLAG pins in ADSP-2156x
  • How to properly invalidate the Pre-Fetch Buffer?
  • How to read the status of SYS_BMODE pins using software for ADSP-21569 and ADSP-21593?
  • How to select PCG Input source for ADSP-SC59x
  • +I2S PCG: FAQ
  • Is it feasible to transition the pins mode from SPI functionality to GPIO after booting the DSP from SPI master?
  • Is it possible to boot the program code from HyperFlash and execute it in HyperRAM?
  • Is it possible to recover the information from Loader(LDR) or executable(DXE) files.
  • Is it possible to use the ADSP-21569 init code for ADSP-21565?
  • Is it possible to use the same pin as SPI_SS as a GPIO interrupt trigger when using SPI simultaneously?
  • +JTAG: FAQ
  • MTM DMA transfer on ADSP-21489
  • Output L and R channels are reversed in AD1939_I2S_Sampled_Based_Talkthru BSP code for ADSP-21469
  • Pre-boot time for ADSP-2156x and ADSP-SC59x/ADSP-2159x
  • Second stage loader example for SC594
  • +SHARC family: FAQ
  • +SHARC processor: FAQ
  • SPI Chain DMA example for ADSP-21489
  • SPI example for ADSP-21369
  • SPI Master to Slave loopback communication in ADSP-21569
  • +SPI serial flash driver: FAQ
  • SSL example for ADSP-21593
  • +SSL: FAQ
  • Support for Automatic Device Detection in Secure Booting
  • Tiny Cache in ADSP-2156x and ADSP-SC59x/ADSP-2159x
  • +USB VID/PID: FAQ
  • Value of DDR reference resistor (DMC0_RZQ) and ZQ for SC594
  • What is the behavior of Circular Buffer mode?
  • What is the difference between “adi_signtool.exe” and “signtool.exe”? Does “adi_signtool.exe” only be used with GLXP?
  • What is the effect of enabling/disabling the ADI_SPORT_BLOCKING_MODE
  • What is the maximum supported clock frequency in Linkport DDR mode for SC594
  • What is the priority of programmable interrupts in comparison to core software interrupts (SFT0I–SFT3I)?
  • What is the Reset value of PADS_PCFG.FAULT_DIS bit ADSP-2159x and SC59x processors
  • What is the SPU_ID for EMDMA0/1 channels in ADSP-SC594/21594
  • Where can I find the 2Mbits memory map configuration for ADSP-21488 automotive parts?
  • Why does the UART TX interrupt trigger before THR and TSR are empty?
  • Why is it mandatory to send 1024-byte blocks during Secure SPI slave boot?

Selective Booting of One Application from Multiple Applications using CCES for ADSP-21479

The default boot kernel will load the application from sector 0. The requirement is to modify the boot kernel in a way that based on a condition (for example, the assertion of a flag input); it should load one of the two applications selectively.

Refer the attached three projects(479_spi, Blink1, Blink2) and follow the below procedure to build and flash:

1. Build the modified kernel 479_spi project to generate the 479_spi.dxe file. Before build, please ensure to build in release configuration( Right click of the project > Build Configurations > Set Active > Choose Release). 479_spi.dxe is available in Release folder.

2. Build the project “Blink1” to generate Blink1.ldr for spi flash boot in ASCII format with loader options, as shown in Figure1. Ensure that it uses the modified kernel 479_spi.dxe.

3. Build the project “Blink2” to generate Blink2.ldr for spi flash boot in ASCII format with loader options, as shown in Figure2. This project may use default boot kernel as its boot kernel will not be used.

4. Use below command to flash "blink1.ldr" in offset 0x0.

cldp -proc ADSP-21479 -emu ICE-1000 -driver "C:\Analog Devices\ADSP-21479_EZKIT-Rel1.0.0\21479_EZ-Board\Examples\Device_Programmer\serial\21479_m25p16_dpia.dxe" -cmd prog -erase all -format ascii -offset 0x0 -file "Blink1.ldr"

5. Use below command to flash "blink2.ldr" in offset 0x2000. Refer Figure3.

cldp -proc ADSP-21479 -emu ICE-1000 -driver "C:\Analog Devices\ADSP-21479_EZKIT-Rel1.0.0\21479_EZ-Board\Examples\Device_Programmer\serial\21479_m25p16_dpia.dxe" -cmd prog -erase affected -format ascii -offset 0x10000 -file "Blink2.ldr"

6. After two LDR files are programmed into flash memory, Set SW4 to 1 for serial and then press the reset button or cycle power to the board.

After reset, the customized boot kernel loads and checks the status of the FLAG1 pin (connected to SW8). If the switch was pressed (FLAG0 = 1), the kernel loads application “Blink2”; otherwise, if FLAG1 = 0, it loads the application “Blink1”.

ADSP_21479.zip

  • Share
  • History
  • More