Post Go back to editing

Unable to set breakpoints in CCES with ADSP-SC589 EZ BRD on DSP cores

Thread Summary

The user encountered an issue where breakpoints could not be set in DSP cores due to missing debug line information, despite the -g compiler option being enabled. The final solution was to re-import the project into a new workspace, which resolved the problem. An accompanying answer suggested this workaround, but the reason why it works was not explained.
AI Generated Content

If I set a breakpoint in one of the DSP cores, when I try to debug I get the error message "Failed to set breakpoint at C:\Users\tchadwick\cces\2.8.0\testCore1_Core1\src\testCore1_Core1.c [line: 26] because there is no debug line info.".  I checked the settings and it says that it should be generating debug information (-g option to the compiler).  I can set breakpoints in the ARM core but can't in either of the DSP cores.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.