Post Go back to editing

A question about the ADSP-21479 be a slave device!

Thread Summary

The user encountered an issue with the ADSP-21479 SPI slave device where it required sending the read command twice to receive the correct data. The problem was resolved by ensuring the master device (Rx-H8) waits for the slave to load the data into the TXSPIB register before sending the next command. The delay was necessary to allow the slave sufficient time to process the read request.
AI Generated Content

Dear All :

               I want the ADSP-21479 be a slave device and the ADSP-21479 can recevice the master command and transfer data to master !

Attached file is my sample code!

My question is I don't know why ? when I send read command I always need send the command twice ans the data value will be correct !

for example :

    To read Data_Temp[2] value(0xcc) ,master send the read command -> 030200

    03 -  INSTR

    02 -  Address                                                         

    00 -  Value - for write command          

                                                            

    // In begin the *pTXSPIB is 0 and  in switch case set *pTXSPIB = Data_Temp[Address] (0xcc)

    // MISO pin measure is 0,but the *pTXSPIB is 0xcc, get fail value(0x00) ?

              

    send the read command aging -> 030200              

    // the *pTXSPIB is 0xcc and in switch case set *pTXSPIB = Data_Temp[Address] (0xcc)

    // MISO pin measure is 0xcc,and the *pTXSPIB is 0xcc, get correct data in this time(0xcc)!

    But, continue to read other Data_Temp value

    To read Data_Temp[0] value(0xaa)     master send the read command -> 030000

              

    // the *pTXSPIB is 0xcc now and  in switch case set *pTXSPIB = Data_Temp[Address] (0xaa)

    // MISO pin measure is 0xcc,but the *pTXSPIB is 0xaa ,get fail value(0xcc) ?

    send the read command aging -> 030000

    // the *pTXSPIB is 0xaa and in switch case set *pTXSPIB = Data_Temp[Address] (0xaa)

    // MISO pin measure is 0xaa,and the *pTXSPIB is 0xaa, get correct data in this time(0xaa)!

    I don't know why I want to get correct data always need to send the master command twice?

    Where is the problem? Who can tell me?

    Thanks !!

Parents Reply Children
No Data