Post Go back to editing

A question about the ADSP-21479 be a slave device!

Dear All :

               I want the ADSP-21479 be a slave device and the ADSP-21479 can recevice the master command and transfer data to master !

Attached file is my sample code!

My question is I don't know why ? when I send read command I always need send the command twice ans the data value will be correct !

for example :

    To read Data_Temp[2] value(0xcc) ,master send the read command -> 030200

    03 -  INSTR

    02 -  Address                                                         

    00 -  Value - for write command          

                                                            

    // In begin the *pTXSPIB is 0 and  in switch case set *pTXSPIB = Data_Temp[Address] (0xcc)

    // MISO pin measure is 0,but the *pTXSPIB is 0xcc, get fail value(0x00) ?

              

    send the read command aging -> 030200              

    // the *pTXSPIB is 0xcc and in switch case set *pTXSPIB = Data_Temp[Address] (0xcc)

    // MISO pin measure is 0xcc,and the *pTXSPIB is 0xcc, get correct data in this time(0xcc)!

    But, continue to read other Data_Temp value

    To read Data_Temp[0] value(0xaa)     master send the read command -> 030000

              

    // the *pTXSPIB is 0xcc now and  in switch case set *pTXSPIB = Data_Temp[Address] (0xaa)

    // MISO pin measure is 0xcc,but the *pTXSPIB is 0xaa ,get fail value(0xcc) ?

    send the read command aging -> 030000

    // the *pTXSPIB is 0xaa and in switch case set *pTXSPIB = Data_Temp[Address] (0xaa)

    // MISO pin measure is 0xaa,and the *pTXSPIB is 0xaa, get correct data in this time(0xaa)!

    I don't know why I want to get correct data always need to send the master command twice?

    Where is the problem? Who can tell me?

    Thanks !!

Parents
  • Hi,

    Thanks for further details. After going through your code and description, I have following question/suggestion:

    After receiving the command, the slave requires some time to fill the required data into the TXSPIB regsiter. Before the TXSPIB register is loaded by the slave, the master should not send another set of 32 SPICLK cycles to read the addressed data. How are you taking care of this delay ? There are two possible ways:

    1) First calculate the time the slave takes after receving the read command to fill the TXSPIB register with the correct data. Use this measured time with enough margin to calculate a worst case time. Then, make sure that after sending the read command, the master sends the next set of 32 SPICLK cycles after this worst case time.

    2) Use a seperate flag signal with which the slave can indicate to the master that the requested data is ready to be read.

    Hope this helps.

    Thanks,

    Mitesh

Reply
  • Hi,

    Thanks for further details. After going through your code and description, I have following question/suggestion:

    After receiving the command, the slave requires some time to fill the required data into the TXSPIB regsiter. Before the TXSPIB register is loaded by the slave, the master should not send another set of 32 SPICLK cycles to read the addressed data. How are you taking care of this delay ? There are two possible ways:

    1) First calculate the time the slave takes after receving the read command to fill the TXSPIB register with the correct data. Use this measured time with enough margin to calculate a worst case time. Then, make sure that after sending the read command, the master sends the next set of 32 SPICLK cycles after this worst case time.

    2) Use a seperate flag signal with which the slave can indicate to the master that the requested data is ready to be read.

    Hope this helps.

    Thanks,

    Mitesh

Children
No Data