Post Go back to editing

ADSP-21363 SPI 32bit 40Mhz problem

Hi

I have a problem with SPI interface at maximum frequency (40MHz).

The problem is as follows:

Code:

                R12 = 0x07900017;

                DM (TXSPI) =  R12;

                nop;

                nop;

                nop;

                ustat4=dm(SPISTAT);

                bit tst ustat4 RXS;//SPIFE;

                IF NOT TF jump (pc,-2);

While configured as  SPIBAUD = 4, i. е. SPICLK=20 MHz RXS bit set’s up properly.

While configured as SPIBAUD = 2, i. е. SPICLK=40 MHz RXS bit doesn’t set’s up at all.

Regarding SPIFE bit it always set up properly.

                SPI configuration:

                USTAT4 = 0x5D05;

                DM (SPICTL) = USTAT4;

Probably this problem is somehow related to 32bit words since if word length is changed to 8bit RSX is set up even at 40MHz.

Any comments on that?

Parents Reply Children
No Data