Post Go back to editing

Using an Emulator to defeat watchdog

Almost all the embedded designs I take credit for detect the presence of, or the operation of an emulator to defeat a watchdog circuit. Obviously when stepping through code, having the processor reset is not much help.
So, for the SHARC processors (ADSP-21065L & ADSP-21160N), the ICE TRST signal is used which goes high when the test port is active and the DSP core paused. Has anyone else done this, what has been your experience - or can you recommend a better way (by the way jumpers and switches or any miss configurable parts are not allowed).
Anyone know a down side to this, perhaps newer processor issues?

 

  • Hi   Stevie,

      Sorry about the delay in getting back. Can you give me more information about what yu are trying to do? It is not clear from the earlier description.

    Thanks

    Deepa

  • Hi Deepa,

    I must be on my 5th design using various SHARC processors, this time I am upgrading an older legacy design which uses the old ADSP21160N part (we want to keep the software as is for now).

    In all my previous designs I have used an external watchdog counter (ASSP or PLD/FPGA) and so it has been convenient for me to use the JTAG emulator port TRST line to hold the watchdog timer reset whilst using the debugger (EZICE). I suspect later DSP variants with internal watchdog do a similar thing.

    Anyway, this is the first time using this older 21160 part and just wanted to double check that the JTAG timing is friendly with this kind of feature and perhaps then to recommend it as an alternative to using test links.

    Regards

    Steve

    Stephen Wells

    Electronics MTS | Implant AGS | Applied Materials

    Office 512-272-3137

    The content of this message is Applied Materials Confidential. If you are not the intended recipient and have received this message in error, any use or distribution is prohibited. Please notify me immediately by reply e-mail and delete this message from your computer system. Thank you.

      • Save a tree. Please don't print this e-mail unless needed.

    From: DeepV analog@sgaur.hosted.jivesoftware.com

    Sent: Monday, September 19, 2011 6:39 AM

    To: Steve Wells

    Subject: New message: "Using an Emulator to defeat watchdog"

    Analog Devices EngineerZone<http://ez.analog.com/index.jspa>

    Using an Emulator to defeat watchdog

    reply from DeepV<http://ez.analog.com/people/DeepV> in SHARC Processors - View the full discussion<http://ez.analog.com/message/32425#32425

  • Hi Stevie,

    I would like to get a clarification regarding your setup. While the emulqtor is being used the TRST line is -pulled high by the emulator. So how does that keep the watchdog in reset?

      I might not be able to answer if the JTAG timing will work with the watchdog. For more information on how to interface you might refer to the JTAG timing specification in the datasheet.

    Also please refer to EE-68, JTAG reference manual for more information , based on which the JTAG connection is implemented.

    Thanks

    Deepa

  • Hi Deepa,

    This is the way my watchdog circuit works:

    I have an external watchdog counter, this is hardware and part of an FPGA.

    The watchdog counter is reset to 0 by:

    1)      The DSP master reset going low

    2)      By the emulators TRST line going high. I have a 4K7 pull down resistor.

    3)      A transition on FLAG3 a general purpose DSP I/O line.

    Under normal operation the counter is reset to 0 by software using the FLAG3 signal.

    The counter has 2 thresholds:

    1)      After 100mS, the first threshold increments a violation counter in the FPGA, asserts a DSP NMI (reports the exception and does some task scheduler checking - stack overflow etc.)

    2)      After a total 200mS, the second threshold asserts DSP reset.

    When the DSP boots, the code can query the FPGA to read some status flags and registers – there are many, here’s 4 . . .

    1)      Manual reset

    2)      Power on reset

    3)      Stack overflow

    4)      Watchdog timeout

    The boot cause status is displayed on boot-up.

    So when an emulator is connected to the JTAG port and TRST is high, the watchdog counter is reset to 0 to allow debugging.

    This works fine on a DUAL ADSP21065L and a similar or more basic version for the ADSP21160N.

    So, if the basic JTAG operation for the ADSP21065L is the same as the ADSP21160N i.e. TRST works in the same way, then the circuit should work ok.

    Regards

    Steve

    Stephen Wells

    Electronics MTS | Implant AGS | Applied Materials

    Office 512-272-3137

    The content of this message is Applied Materials Confidential. If you are not the intended recipient and have received this message in error, any use or distribution is prohibited. Please notify me immediately by reply e-mail and delete this message from your computer system. Thank you.

      • Save a tree. Please don't print this e-mail unless needed.

    From: DeepV analog@sgaur.hosted.jivesoftware.com

    Sent: Monday, October 03, 2011 5:04 AM

    To: Steve Wells

    Subject: New message: "Using an Emulator to defeat watchdog"

    Analog Devices EngineerZone<http://ez.analog.com/index.jspa>

    Using an Emulator to defeat watchdog

    reply from DeepV<http://ez.analog.com/people/DeepV> in SHARC Processors - View the full discussion<http://ez.analog.com/message/33422#33422

  • Hi Steve,

       The implementation of JTAG hastn changed from ADSP -2106x processors to the newer processors. So i feel that if you were able to successfully implement the above mentioned system in the ADSP-2106x you should be able to do the same in the newer processors.

    Other than that with the information provided, i dont see any other issues.

    Thanks

    Deepa

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin