ADSP-21364 and SIG_GPTMR2

Hi,

According to Visual DSP++ 4.0 Compiler and Library Ref Manual, SIG_GPTMR2 processor signal is only supported with ADSP-2126x.

However, I'm working with ADSP-21364 and I have a program using SIG_GPTMR2, which seems to work fine.

SIG_GPTMR2 is the General purpouse IOP timer 2 which should be SIG_P17 in the case of ADSP-21364.

My question is: Is it right to use SIG_GPTMR2 with ADSP-21364? How can this be working?

Thanks,

Imanol

Parents
  • 0
    •  Analog Employees 
    on Aug 24, 2011 3:39 PM

    Hi Imanol,

    Your observations are expected. The reason is that though the VisualDSP++ library manual doesn't explicitly mention the signal name SIG_GPTMR2, the "signal.h" header file still has the corresponding definition:

    #if defined(__ADSP21367__) || defined(__ADSP21368__) || defined(__ADSP21369__) || defined(__2137x__) || defined(__214xx__)
    # define SIG_EP0        20 // External Port0 interrupt - Corresponds to Sig_P9
    # define SIG_GPTMR1     21
    # define SIG_SP7        22 // SPORT 7 interrupt - Corresponds to Sig_P11 in LX3
    # define SIG_DAIL       23
    # define SIG_EP1        24 // External Port1 interrupt - Corresponds to Sig_P13
    # define SIG_DPI        25 // DPII interrup -Corresponds to Sig_P14 in LX3
    # define SIG_MTM        26 // Mem to Mem Interrupt - Corresponds to Sig_P15
    # define SIG_SP6        27 // SPORT 6 interrupt -Corresponds to Sig_P16 in LX3
    # define SIG_GPTMR2     28         
    # define SIG_SPIL       29         
    #else
    # define SIG_PP         20
    # define SIG_GPTMR1     21
    # define SIG_DAIL       23
    # define SIG_PWM        24
    # define SIG_DTCP       26
    # define SIG_GPTMR2     28         
    # define SIG_SPIL       29         
    #endif

    Please note that unlike in ADSP-2126x,  in ADSP-2136x the P17I interrupt (mapped to GPTMR2 by default)  can be mapped to any interrupt other than GPTMR2.  Using the signal name "SIG_GPTMR2" will have the same effect of using the signal name "SIG_P17I". However, the recommended way is to first make sure that the PICRx registers are programmed appropriately to map the GPTMR2 interrupt to the required programmable interrupt (PxI) and then use the definition (SIG_PxI) instead of SIG_GPTMR2. 

    Hope this helps.

    Thanks,

    Mitesh

    PS:: I would also recommend you to use the latest VisualDSP++ version (5.0) with the latest update (Update 9.1) available at the link below:

    http://www.analog.com/en/processors-dsp/software-and-reference-designs/content/visualdsp_tools_upgrades/fca.html


Reply
  • 0
    •  Analog Employees 
    on Aug 24, 2011 3:39 PM

    Hi Imanol,

    Your observations are expected. The reason is that though the VisualDSP++ library manual doesn't explicitly mention the signal name SIG_GPTMR2, the "signal.h" header file still has the corresponding definition:

    #if defined(__ADSP21367__) || defined(__ADSP21368__) || defined(__ADSP21369__) || defined(__2137x__) || defined(__214xx__)
    # define SIG_EP0        20 // External Port0 interrupt - Corresponds to Sig_P9
    # define SIG_GPTMR1     21
    # define SIG_SP7        22 // SPORT 7 interrupt - Corresponds to Sig_P11 in LX3
    # define SIG_DAIL       23
    # define SIG_EP1        24 // External Port1 interrupt - Corresponds to Sig_P13
    # define SIG_DPI        25 // DPII interrup -Corresponds to Sig_P14 in LX3
    # define SIG_MTM        26 // Mem to Mem Interrupt - Corresponds to Sig_P15
    # define SIG_SP6        27 // SPORT 6 interrupt -Corresponds to Sig_P16 in LX3
    # define SIG_GPTMR2     28         
    # define SIG_SPIL       29         
    #else
    # define SIG_PP         20
    # define SIG_GPTMR1     21
    # define SIG_DAIL       23
    # define SIG_PWM        24
    # define SIG_DTCP       26
    # define SIG_GPTMR2     28         
    # define SIG_SPIL       29         
    #endif

    Please note that unlike in ADSP-2126x,  in ADSP-2136x the P17I interrupt (mapped to GPTMR2 by default)  can be mapped to any interrupt other than GPTMR2.  Using the signal name "SIG_GPTMR2" will have the same effect of using the signal name "SIG_P17I". However, the recommended way is to first make sure that the PICRx registers are programmed appropriately to map the GPTMR2 interrupt to the required programmable interrupt (PxI) and then use the definition (SIG_PxI) instead of SIG_GPTMR2. 

    Hope this helps.

    Thanks,

    Mitesh

    PS:: I would also recommend you to use the latest VisualDSP++ version (5.0) with the latest update (Update 9.1) available at the link below:

    http://www.analog.com/en/processors-dsp/software-and-reference-designs/content/visualdsp_tools_upgrades/fca.html


Children
No Data