Post Go back to editing

Split booting from slave and master SPI

Hi all,

I read some relevant documents on SPI bootloaders and still am a bit puzzled on this.

From my point of view, it is possible what I want to achieve, but the amount of information on this is too big as to be sure not to miss something.

I'd like to do the following thing:

1. Provide the initial bootloader (256 48-bit words) from a host microcontroller (SPI master) to an ADSP 21261 processor (SPI slave)

2. Boot the application from a serial flash with the DSP as SPI master

The first 256 words are received from the microcontroller since the BOOT_CFG flags are configured for SPI slave.

The code in the bootloader can use SPI master to get the application code from a serial flash connected to the SPI port.

Correct?

The microcontroller is a rather small one with limited amount of on-chip flash memory.

Any comments on this?

Thanks in advance,

Rainer

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.