Post Go back to editing

UART Data transfer using DMA

Thread Summary

The user encountered a linking error and issues with UART DMA transfer on the ADSP-21489 EZ-KIT. The problem was resolved by ensuring the baud rate was correctly set to 19200 on both the DSP and PC. For continuous data transfer, the user was advised to use UART DMA chaining mode and verify the UART settings and signal integrity with an oscilloscope.
AI Generated Content

Dear Sir,

Please provide me an example code in C for the above requirement. When I'm modifying the UART echo example for core interrupt to DMA interrupt during linking it shows error in IDDE as fatal error : Link failed and The following symbols referenced in processor "P0" could not be resolved: 'length[_length]' referenced from '.\Debug\UARTDMA transfer.doj'

please help in this regard as soon as possible.

regards

satya

Parents
  • Hi Satya,

                In this code the UART signals are directly looped back on the SRU. There is no external connection needed. The jumper settings also should not affect anything.

    1. Did you check the memory buffers tx_data1 and rx_data1? Is there any data received in the rx_data1?

    2. Can you place a breakpoint inside the ISR and check?

    3. Can you capture the UART registers after running your code and send to me?

    Regards,

    Jeyanthi

Reply
  • Hi Satya,

                In this code the UART signals are directly looped back on the SRU. There is no external connection needed. The jumper settings also should not affect anything.

    1. Did you check the memory buffers tx_data1 and rx_data1? Is there any data received in the rx_data1?

    2. Can you place a breakpoint inside the ISR and check?

    3. Can you capture the UART registers after running your code and send to me?

    Regards,

    Jeyanthi

Children
No Data