Post Go back to editing

UART Data transfer using DMA

Thread Summary

The user encountered a linking error and issues with UART DMA transfer on the ADSP-21489 EZ-KIT. The problem was resolved by ensuring the baud rate was correctly set to 19200 on both the DSP and PC. For continuous data transfer, the user was advised to use UART DMA chaining mode and verify the UART settings and signal integrity with an oscilloscope.
AI Generated Content

Dear Sir,

Please provide me an example code in C for the above requirement. When I'm modifying the UART echo example for core interrupt to DMA interrupt during linking it shows error in IDDE as fatal error : Link failed and The following symbols referenced in processor "P0" could not be resolved: 'length[_length]' referenced from '.\Debug\UARTDMA transfer.doj'

please help in this regard as soon as possible.

regards

satya

Parents
  • Hi Jeyanthi,

    thanks for your reply and code.

    Can you specify the testing method of your code to verify it.

    When I load your code in the ADSP-21489 EZ-KIT for verifying, i didn't see the result when I monitored the uiDMA_count variable. since during every receive it enables ISR corresponding it updates the uiDMA_count variable.

    regards

    satya

Reply
  • Hi Jeyanthi,

    thanks for your reply and code.

    Can you specify the testing method of your code to verify it.

    When I load your code in the ADSP-21489 EZ-KIT for verifying, i didn't see the result when I monitored the uiDMA_count variable. since during every receive it enables ISR corresponding it updates the uiDMA_count variable.

    regards

    satya

Children
No Data